Part Number: CC2564C
Tool/software: Linux
Hi team,
i tried to initialise the Bluetooth device using 6 different bts files I am getting error as below
hciattach /dev/ttyMSM1 texas 115200 flow
Initialization timed out.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2564C
Tool/software: Linux
Hi team,
i tried to initialise the Bluetooth device using 6 different bts files I am getting error as below
hciattach /dev/ttyMSM1 texas 115200 flow
Initialization timed out.
Are you using a launchpad for this test setup? The timeout is usually because of improper connections to the device. Please verify you have connected the device correctly to the XDS110.
BR,
Vince
we are not using luanchpad we are using IPQ40XX processor
| PROCESSOR Board | CC2564C EVK |
| TX | RF1 - P9 |
| RX | RF1 - P7 |
| GND | RF2 - P2 |
| VDD | RF2 - P7 |
| RTC | RF1 - P3 |
| CTC | RF2 - P18 |
this the host to CC2564C connection please if i did any wrong ? please correct that one.
please suggest me which bts file is for CC2564C.
This generally means an issue with UART connection to the BT controller. Please, check the pin muxes and the UART connection is proper to the controller.
Thanks