Part Number: CC2642R
Tool/software: TI C/C++ Compiler
I'm trying to build an application using GNU makefile + GCC.
However during the link I've got the follow error:
ti/drivers/UART.c:92: undefined reference to `HwiP_disable'
ti/drivers/UART.c:103: undefined reference to `HwiP_restore'
ti/drivers/UART.c:104: undefined reference to `UART_config'
ti/drivers/UART.c:104: undefined reference to `UART_count
I'm adding the following libraries the link:
- source/ti/drivers/lib/drivers_cc26x2.am4fg;
- source/ti/devices/cc13x2_cc26x2/driverlib/bin/gcc/driverlib.lib.
But the error persist. I also ran the command "nm" with the libraries and I've realized that the library "drivers_cc26x2.am4fg" have the symbols but they appear as "U" (Undefined).
$ nm source/ti/drivers/lib/drivers_cc26x2.am4fg | grep UART_c
00000001 T UART_close
U UART_config
00000001 T UART_control
U UART_count
What is actually the correct library?