This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BLE-STACK: BLE Advertisement Payload (31 bytes on the primary channels)

Part Number: BLE-STACK

Hello,

Can I change the contents of the payload for each new advertisement .


For example : I transmit a ibeacon packet on channel 37,38,39. Then the next advertising is a custom packet on channel 37,38,39.

I want to keep alternating between these two packets. I’ve posted the same on the e2e forum and would be glad if you can share your thoughts on the same.

Will the protocol stack allow me to do the same.

If not could you suggest alternatives to  this.

Kindly let me know.

Thanks