The whole new project only adds the "test" part and removes the IAR pre-compiled POWER_SAVING macro definition. After compilation, it is burned into the chip for observation. The chip is reset once every second during simulation. There is no response during non-simulation, but use 1.4. The repository does not have this problem. Is this really a new version of the bug?
Found this problem is to use a BLE-CC254x-1.5.0.1 repository in a new project, the program has been added to the watchdog, but there will be a crash, the crash phenomenon is not found in Bluetooth, the serial port does not work, the button does not respond The whole chip does not know what state it is, but the previous version 1.4 has never tested this problem. If the 1.4 version of the watchdog is removed in time, there will be no crash. At first, I thought it was a problem after modifying the program. A library program test watchdog that has not changed anything, there is no response, please answer the master! ! ! ! !