Other Parts Discussed in Thread: CC2541, , TPS62730
I have a working project that uses a CC2541, but really want to be using a part with a higher temperature rating.
The CC2541-Q1 is rated to 105 degrees, whereas the CC2541 is only rated to 85 degrees.
I can't find anything that says these parts are identical, and likewise can't find any description that details any differences between these two devices.
Can I use a CC2541-Q1 in the place of a CC2541?