This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: Hidden files within SDK needed to compile code?

Part Number: LAUNCHXL-CC26X2R1

Hello,

I'm trying to store the Simplelink SDK (version 3.10.01.11) into our configuration management tool (ClearCase), but am running into issues with adding some of the files. When copying the SDK over, a bunch of hidden files were also copied over. (.vers_b200, .vers_g200, .vers_r200, .xdc-F09, and various others) These files are empty (0 bytes), and ClearCase doesn't allow empty files to be added to source control. These files are scattered throughout the kernel directory and the xdctools directory. Are these files needed to compile the code properly? Can I delete them without any negative side effects?

Thanks.