Part Number: CC2650MODA
Other Parts Discussed in Thread: CC2650
Hi expert,
When a moisture-proof coating material is applied to CC2650 MODAMOHT below conditions,
Is there any adverse effect on radio communication?
conditions;
1. Moisture-proof coating is non-conductive.
2. The coating area is 3 side areas and 1 front area.
3. Will not apply to the antenna section.
We think that the following points are assumed, but how is it?
・ Matching may occur when applying to antenna, transmission line between chips.
・ However, because it is the 2.4 GHz band, the influence is considered to be small when considered from the wavelength.
Regards,