This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: Configuration of CC2642R for BLE 5.0 and long range - AT commands ; advertising

Part Number: CC2642R


Hi All,

I am proposing CC2642R to my customer in the module package offered by BLE, our 3rd party.

Product Line recommended me to ask in e2e these questions below:

 • Is it possible to change the configuration (for example switch from the long range configuration to the standard 2Mbps configuration of the module also via firmware and not only via AT commands)?

• Possibility to change the data field from advertising to transmission and then on receiving being able to have these data at the application level in order to be processed?

I would just like to use advertising to communicate between the modules (is it feasible?)

• Information on how to certify the module?

• If there are any example firmware on the web?

Many Thanks,

Antonio

 

Customer NICE is very interested at this solution, but they do not have any know-how about BLE 5.0 module. BDE already shipped the module to NICE.

 

Many Thanks,