We developed a device using the CC2564MODx. We did not add any extra Hardware regarding communications and data transmission.
Our doubt is that, we want to sell our device in some countries, and the certification company we usually work with told us that we have to perform Conducted testing and Radiated testing for some countries. We thought that this module was worldwide certified. Is it still needed to do some testing for certifications in other countries, even if the module is already certified in them?
The fact is that the only thing we do for this testing is to connect a SMA antenna connector and run the Texas' test mode, which we think is already tested, and does not make sense to repeat the same test it in each country.
Thank you for your attention.