Tool/software: Code Composer Studio
I checked current SDK sample for cc2640r2f and noted that 2.405GHz is its minimum frequency.
Is this true? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I checked current SDK sample for cc2640r2f and noted that 2.405GHz is its minimum frequency.
Is this true? Thanks.
According to the frequency table below from config.c, what is the setting for 2.36GHz? Does the documentation open to public download? Thanks.
FrequencyTableEntry config_frequencyTable_2_4[] =
{
{ "2405 ", 0x0965, 0x0000, 0x0 },
{ "2410 ", 0x096a, 0x0000, 0x0 },
{ "2415 ", 0x096f, 0x0000, 0x0 },
{ "2420 ", 0x0974, 0x0000, 0x0 },
{ "2425 ", 0x0979, 0x0000, 0x0 },
{ "2430 ", 0x097e, 0x0000, 0x0 },
{ "2435 ", 0x0983, 0x0000, 0x0 },
{ "2440 ", 0x0988, 0x0000, 0x0 },
{ "2445 ", 0x098d, 0x0000, 0x0 },
{ "2450 ", 0x0992, 0x0000, 0x0 },
{ "2455 ", 0x0997, 0x0000, 0x0 },
{ "2460 ", 0x099c, 0x0000, 0x0 },
{ "2465 ", 0x09a1, 0x0000, 0x0 },
{ "2470 ", 0x09a6, 0x0000, 0x0 },
{ "2475 ", 0x09ab, 0x0000, 0x0 },
{ "2480 ", 0x09b0, 0x0000, 0x0 },
If you are working with prop RF it's no need to use a preconfigured frequency table, ref the rf examples under TI drivers: http://dev.ti.com/tirex/explore/node?node=APwBWdtqTgxZuJ9l4iRqpQ__krol.2c__LATEST
You should be able to make your own table based on your needs.