Part Number: CC2564MODN
Tool/software: Linux
Hi,
I am working with IMX6ULL connect to CC2564MODN through UART. I have 'protocol not suppoted' problem.
My Bluz version is : v5.49.
what is correct hciattach command ?
when I write :
hciattach -t 30 -s 115200 /dev/ttymxc1 texas 115200
Found a Texas Instruments' chip!
Firmware file : /lib/firmware/ti-connectivity/TIInit_6.7.16.bts
Loaded BTS script version 1
texas: changing baud rate to 115200, flow control to 1
Setting TTY to N_HCI line discipline
Can't set device: Protocol not supported
Can't initialize device: Protocol not supported
when I write:
root@imx6ull14x14evk:~# hciattach /dev/ttymxc1 texas 115200 flow
Found a Texas Instruments' chip!
Firmware file : /lib/firmware/ti-connectivity/TIInit_6.7.26.bts
can't open firmware file: No such file or directory
Warning: cannot find BTS file: /lib/firmware/ti-connectivity/TIInit_6.7.26.bts
Setting TTY to N_HCI line discipline
Can't set device: Protocol not supported
Can't initialize device: Protocol not supported
In the first case Bluez search TIInit_6.7.16.bts file, in the second case Bluez search TIInit_6.7.26.bts.
what is the correct command ?
what is the correct .bts file ?
where I found the correct file ?
Can someone help me ?
Sergio.