Tool/software: TI-RTOS
Hi to everybody,
I have two open questions which I'm not able to solve..
I'm working with CC2642 and simplelink_cc13x2_26x2_sdk_2_40_00_81.
I'm using a SPhone as a Master and a peripheral board (multi_role software based).
First question:
After a succesfull bonding through password request, if I drop the connection through the SPhone, I will never be able to find (with a new scan) the peripheral again (the drop connection is recognize corretly from the peripheral).
The only ways I'm able to find it again is powering OFF-ON the peripheral or reflashing it.
However I have noticed this behaviour using Samsung S4 mini: if I use Huwawei Mate 20 Pro the peripheral still be visible even after a succesfull bonding and its first disconnection.
I remeber there was a similar issue with CC2642 and SDK 1_35_00_33, fixed later with a new SDK version...
Anyway, do you have any idea or suggestion to avoid this problem with some SPhone ?
Second question:
With every SPhone I have tryied, if I delete into the SPhone the bonding made with the peripheral and I try a new connection between the SPhone and peripheral, there isn't any password request event from SPhone side AND there isn't any pairing event from Peripheral side during the connection(once bonded with a SPhone I should receive at least the GAPBOND_PAIRING_STATE_ENCRYPTED for every connection made with it).
It seems like the bonding is saved into the peripheral even if i've delete it from SPhone side...
How is possible to avoid this behaviour?
Many thanks in advance,
Federico