This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2640R2: Add oad to multi role of simplelinkacademy

Part Number: LAUNCHXL-CC2640R2


Hi

I test "add oad to multi role" of simplinkacademy

"http://dev.ti.com/tirex/explore/node?node=AJ3HKMayaRkezRxrWedgQA__krol.2c__LATEST"

My compiler is IAR(8.40.1)

SDK is simplelink_cc2640r2_sdk_3_10_00_15.

We used the Cache as GPRAM option to increase the number of MAX_NUM_BLE_CONNS.
However, when using Cache as GPRAM, the following error message is issued.
I add CACHE_AS_RAM predefine option and CACHE_AS_RAM=1 link define option.

If you do not use Cache as GPRAM, you are downloading and working well.
What's the problem?
"Mon Aug 05, 2019 11:40:41: Fatal error: Failed to do go: (Error -2134 @ 0x0) If error persists, confirm configuration, power-cycle the board, and / or try more reliable JTAG settings (eg lower TCLK). (Emulation package 8.1.0.00005)
Session aborted! "
Br
yj Kim