This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SIMPLELINK-CC2640R2-SDK: 2.40: Simple Central not able to connect to 2 Simple Peripheral Device?

Part Number: SIMPLELINK-CC2640R2-SDK

Hi,

I am trying to connect 2 CC2640R2F Launchpad with Simple Peripheral Program to 1 CC2640R2F Launchpad Simple Central. From what I read I can connect 8 BLE Devices to Simple Central. But when I try the Simple Central what happens I connect to the first CC2640R2F Launchpad. I need to disconnect the first CC2640R2F Launchpad, if I want to connect to the second CC2640R2F Launchpad. This does not demonstrate multiple BLE Peripheral Devices connected to 1 Simple Central Device.

Do you have example code or program that able to connect 1-8 BLE Peripheral Devices to 1 Simple Central Device?

-kel