Part Number: LAUNCHXL-CC26X2R1
Hi
We have some questions about Simple NV:
1. In project_zero.c, it uses the Simple NV to store the "Service changed flag"(after receiving "OAD_COMPLETE_EVT" ), but it seems no one to access it, could you help to double check it? May I comment out this portion of code?
2. About customer NV, the range is 0x80 - 0x8F, does it means I have the 16 locations to store data? What is the size of the data that can be stored on each locations(ID)?
3. Do you have any tools to read/write/erase the Simple NV area?
4. What is the maximum size of customer NV? we would like to store 16KB user data, do you have any suggestions to me?
SDK Version: simplelink_cc13x2_26x2_sdk_3_20_00_68
Thanks.
BR
Trevor