Part Number: CC2564C
Team,
I got an inquiry about supported feature of the CC2564C from my customer.
According to “Erratum 10734: Pairing Updates”, Read Local Simple Pairing Options Command would be added as new command. And the support commands table also modified that this feature assigns at Octet 41: Bit 3. However, it seems the CC2564C cannot be assigned this feature.
Here is the HCI log for CMD_CMP of the read_Local_commands_command. The table Octet 41/ Bit 3 was ‘0’.
----
Received HCI-EVT: HCI_COMMAND_COMPLETE [Length 68]
NumHCICommandPackets:1 Command:HCI_READ_LOCAL_COMMANDS
Status:SUCCESS
ff ff ff 03 ce ff ff ff 0f ff ff 1f f2 0f e8 fe ................
3f f7 8f ff 1c 00 00 00 61 f7 ff ff 7f 38 00 00 ?.......a....8..
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
----
Does the CC2564C support "Read Local Simple Pairing Options Command"?
Regards,
Nonaka