Part Number: CC2650MODA
Tool/software: Code Composer Studio
Hi,
There is no error in the below program but output pin (DIO2) is not high. What is the reason for no output.?
(In 1st commented line) Is it possible to write values to hardware registers directly in ccs? If so, How can we do?
#include <driverlib/ioc.h>
#include<driverlib/ioc.c>
int main(void)
{
// IOCFG1 = 0x30;-----(1)
// IOCPortConfigureSet(IOID_2, IOC_PORT_GPIO, IOC_STD_OUTPUT);
IOCPinTypeGpioOutput(IOID_2);
GPIO_writeDio(2,1);
BIOS_start();
return 0;
}