This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2642R: CC2642 I2S

Part Number: CC2642R


Tool/software: Code Composer Studio

Hi,

     Does CC2642R I2S work at master mode? If so then which pins of GPIO need to connect for I2S interface in CC2642R.

  • Hi,

    Yes, I2S can be set in master mode on CC2642R. The example i2secho stored in your SDK (examples\rtos\CC26X2R1_LAUNCHXL\drivers\i2secho) shows how to do so.

    The I2S interface requires two clocks: the word clock (WS) and the bit clock (SCK). In addition you can have up to two data lines (SD0 and SD1): each data line can be set to be an input or an output. To finish, the m-clock can be turned on but it is generally not necessary. More details are available in the I2S documentation, in your SDK (docs/tidrivers/doxygen/html/_i2_s_8h.html).

    I hope this will help,

    Best regards,