This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Auto-script RF testing using CWM500 with CC2640R2F in SDK-3.10.00.15

Part Number: CC2640R2F


Hi all,

CWM500 have a feature doing BLE5 RF auto-script testing between 4 different phy(1M, 2M, S2, S8). But 
we found the CWM500 can not initiate the RF testing besides 1M and have question about the TI BLE5 HCI
layer can not fully support  the CWM500.

And I knew we could use the vendor-specific HCI command(0xFC03)(EnhancedTxModemTest) in the SDK to do
the RF testing between different phy.

My question has two:
#1 Is there any standard(not vendor-specific) HCI command that could be used to do the RF testing like 0xFC03
in SDK-3.10.00.15?

#2 If #1 answer is no, should we ask the CWM500 instrument vendor to support the 0xFC03 HCI command to do
the RF testing?

Thanks for reply.

BR,
George