This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: looking for the example

Part Number: CC2640R2F

Dear Sir?Madam,

i'm looking for an example in CC2640R2F SDK (2_40_00_32) version. the concept is that i have to make to devices for the transmission and receiver so for the both functionality i'm using one CC2640R2F as master or one CC2640R2F as master.so idea is like i have send some data from the master to slave so for that i have connect two devices automatically and if connection has been lost i have re-connect both device and that also suppose be done via auto-reconnect functionality.

So is there any example available ? so i can use that example for master and slave.