Part Number: CC2640R2F
Tool/software: Code Composer Studio
Hi,
Recently I am experiencing paring error code 04 a lot, when I am testing my devices. According to the source code the error is SMP_PAIRING_FAILED_CONFIRM_VALUE.
Can someone explain me, what the problem is during paring.
Edit:
The interesting thing is, that I am using the same firmware on different devices and at some devices no pairing error occurs and other ones it does!!
For testing the connection, I am using my IPhoneSe and the LightBlue App.
The firmware is a modified version of the original ProjectZero tutorial code.
The Bond Manager Init is:
uint32_t passkey = 0; // passkey "000000" uint8_t pairMode = GAPBOND_PAIRING_MODE_WAIT_FOR_REQ; uint8_t mitm = TRUE; uint8_t ioCap = GAPBOND_IO_CAP_DISPLAY_ONLY; uint8_t bonding = FALSE;
Thank you
Christian