Part Number: CC2541
Hello,
i'm developing using IAR for CC2541. Need a delay function in the simplebleperipheral project, I read about HalLcd_HW_WaitUs () function but i cant find it.
Can anyone help, please
Regards,
Vito
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2541
Hello,
i'm developing using IAR for CC2541. Need a delay function in the simplebleperipheral project, I read about HalLcd_HW_WaitUs () function but i cant find it.
Can anyone help, please
Regards,
Vito
Hi Joakim,
I created the event and used the osal_Start_timerEx function, but it doesn work. Im developing using simple ble peripheral project on cc2541. After 10 seconds of advertising (general mode) i have to toggle a gpio pin. So I inserted the function
osal_start_timerEx( simpleBLEPeripheral_TaskID, SBP_DONE_EVT, SBP_DONE_EVT_PERIOD )
in the GAPROLE_ADVERTISING case to generate a 10 seconds timer. (#define SBP_DONE_EVT_PERIOD 10000)
Then i created the event, similar to the periodic event:
if ( events & SBP_DONE_EVT )
{
// Restart timer
if ( SBP_DONE_EVT_PERIOD )
{
osal_start_timerEx( simpleBLEPeripheral_TaskID, SBP_DONE_EVT, SBP_DONE_EVT_PERIOD );
P1_7 = 1; //GPIO pin toggle after 10 seconds
}
return (events ^ SBP_DONE_EVT);
}
Can you help me please?
Regards,
Vito