This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2652R: Best way to debug device hang

Part Number: CC2652R

Tool/software: Code Composer Studio

Hello,

I am trying to debug a hang using the CC2652R1 (a Cortex M4 part). I am using TI/RTOS with multiple task threads and I can run in the debugger. Occasionally the device hangs or crashes. I have the assert handler registered but I never see any assert output:

/* Register Application callback to trap asserts raised in the Stack */
  RegisterAssertCback(AssertHandler);

The handler uses Display_print0. Throughout my code I use Display_printf() to print to the UART which all works until the hang and then no more output comes to the UART display.

I also tried running the ROV. It does run and seems to connect but if I use the Task view (for example to see what is going on) I get this error (even if the program is running fine in the debugger, not hung or crashed): 

Error: java.lang.Exception: Target memory read failed at address: 0x200050b4, 

length: 76 This read is at an INVALID address according to the application's section map.

The application is likely either uninitialized or corrupt.

I also tried the Trace view, but it just says "Please select a connected target that supports Trace."

Are there things to do to correct these issues or is there a better way to see where the process is hanging or crashing? 

I'm using CCS 9.1.0.

Thanks for your help!