This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640: bonding, reconnection, Galaxy Note10

Part Number: CC2640

Hi

I use cc2640f128 with my custom board, sdk 2.2.2.

I have reconnection fail issues of "Galaxy Note 10" after bonding. (Paring method : Numeric Comparison)

By the way, this issue is occurred when the Note10 is second device boded to the cc2640.

When the Note10 is first phone after firmware image is downloaded to CC2640, there is no problem.

But after another Note10 or S10 5G is bonded first, the issue is occurred.

I guess the chipset of Note10, S10 5G have some bugs about BLE Bonding Logic.

And I also guess the BLE public mac addresses of the chipsets are same.

So when re-connecting, cc2640 maybe misunderstand that 1st data of bonding list is the information of the device.

I wonder that my guess is right and there is some work-around solution or not.

I captured packets when re-connection fail as below.

Thanks all.