Part Number: CC2564MODA
Other Parts Discussed in Thread: CC2564
We have Linkit 7688 processor with CC2564 for bluetooth connectivity.
UART0 is used as the communication interface.
"hciattach /dev/ttyS0 any 115200" - this command is used to setup the device.
But the result is given below:
[ 1524.147679] Bluetooth: hci0 command 0x1003 tx timeout
[ 1526.227508] Bluetooth: hci0 command 0x1001 tx timeout
[ 1528.307489] Bluetooth: hci0 command 0x1009 tx timeout
The status hciconfig shows the status of the bluetooth as DOWN.
Please help.
Regards,
Ameesh