This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: compilation error on iar using simplelink sdk example simple peripheral

Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2650

Hi,

I tried comiling simple peripheral example of the simple link sdk simplelink_cc2640r2_sdk_3_30_00_20 on iar 8.32.2 . The compiler is showing error as mentioned below.

Error while running "C:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\..\xdctools_3_51_03_28_core\xs"
--xdcpath="C:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\kernel\tirtos\packages;C:\ti\
simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source;C:\ti\simplelink_cc2640r2_sdk_3_30_00_20\
examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack" iar.tools.configuro -c "C:\Program Files (x86)\IAR Systems\Embedded
Workbench 8.2\arm" --cc "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\bin\iccarm.exe" --device "CC2640R2F" --compileOptions "dummy.c -D
BOARD_DISPLAY_USE_LCD=0 -D BOARD_DISPLAY_USE_UART=1 -D BOARD_DISPLAY_USE_UART_ANSI=1 -D CC2640R2_LAUNCHXL -D CC26XX -D CC26XX_R2 -D
DeviceFamily_CC26X0R2 -D xDisplay_DISABLE_ALL -D ICALL_EVENTS -D ICALL_JT -D ICALL_LITE -D ICALL_MAX_NUM_ENTITIES=6 -D ICALL_MAX_NUM_TASKS=3 -D
ICALL_STACK0_ADDR -D MAX_NUM_BLE_CONNS=1 -D POWER_SAVING -D STACK_LIBRARY -D USE_ICALL -D xdc_runtime_Assert_DISABLE_ALL -D xdc_runtime_Log_DISABLE_ALL
--diag_suppress Pa050 -o C:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\FlashROM_StackLibrary\Obj --debug
--endian=little --cpu=Cortex-M3 -f C:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\
config\build_components.opt -f C:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\
config\factory_config.opt -f C:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\tirtos\build_config.opt -f C:\ti\
simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\config\configPkg\compiler.opt.defs -e --fpu=None --dlib_config \"C:\
Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\inc\c\DLib_Config_Normal.h\" -I C:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\blestack\
simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\controller\cc26xx_r2\inc\ -I C:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\blestack\

And

when i start frist time then show

[Su007]: Unable to open the command file "C:\ti\simplelink_cc2640r2_sdk_3_20_00_21\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\config\configPkg\                                 C:\Users\44383\AppData\Local\Temp\EWED4F.tmp 1  

  • Hi,

    Assigning an expert to follow up.

  • Hi Bhanu,

    Regarding the following error message, it's a known impact in IAR and you can disregard it. You should still be able to buid and run the project.

    "[Su007]: Unable to open the command file..."

    I just tested and I am able to build simple peripheral. Did you remember to build the stack project before the app project?

  • Hi,

    I have encountered the same problem.

    I try to compile the stack first. it is work fine.

    then i try to compile app. it failed.

    follow is error message.   IAR 8.23   SDK   3_30,  project :D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral

    Error while running "D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\
    tirtos\iar\app\..\..\..\..\..\..\..\..\..\xdctools_3_51_03_28_core\xs" --xdcpath="D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\
    examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\kernel\tirtos\packages;D:\
    ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\
    ..\..\..\..\source;D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\
    tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\ble5stack" iar.tools.configuro -c "D:\Program Files (x86)\IAR Systems\
    Embedded Workbench 8.2\arm" --cc "D:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\bin\iccarm.exe" --device
    "CC2640R2F" --compileOptions "dummy.c -D DeviceFamily_CC26X0R2 --diag_suppress Pa050 -o D:\ti\
    simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\
    FlashROM_StackLibrary\Obj --debug --endian=little --cpu=Cortex-M3 -f D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\
    CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\defines\cc2640r2lp_app_FlashROM_StackLibrary.opt -f D:\ti\
    simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\
    ..\..\..\source\ti\ble5stack\config\build_components.opt -f D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\
    CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\ble5stack\config\
    factory_config.opt -f D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\
    tirtos\iar\app\..\..\..\tirtos\build_config.opt -f D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\
    ble5stack\simple_peripheral\tirtos\iar\app\..\config\configPkg\compiler.opt.defs -e --fpu=None --dlib_config \"D:\Program
    Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\inc\c\DLib_Config_Normal.h\" -I D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\
    examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\ble5stack\
    controller\cc26xx\inc\ -I D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\ble5stack\inc\ -I D:\ti\
    simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\
    ..\..\..\source\ti\ble5stack\common\cc26xx\ -I D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\
    ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\src\app\ -I D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\
    CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\ble5stack\icall\inc\ -I D:\ti\
    simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\
    ..\..\..\source\ti\ble5stack\inc\ -I D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\ble5stack\profiles\dev_info\ -I D:\ti\
    simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\
    ..\..\..\source\ti\ble5stack\profiles\simple_profile\ -I D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\
    CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\ble5stack\profiles\
    simple_profile\cc26xx\ -I D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\ble5stack\target\ -I D:\ti\
    simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\
    ..\..\..\source\ti\ble5stack\hal\src\inc\ -I D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\
    ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\ble5stack\hal\src\target\_common\ -I D:\ti\
    simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\
    ..\..\..\source\ti\ble5stack\hal\src\target\_common\cc26xx\ -I D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\
    CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\ble5stack\hal\src\target\
    cc2650\rom\ -I D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\
    iar\app\..\..\..\..\..\..\..\..\source\ti\ble5stack\heapmgr\ -I D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\
    CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\ble5stack\icall\src\inc\ -I
    D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\
    ..\..\..\..\..\source\ti\ble5stack\osal\src\inc\ -I D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\
    ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\ble5stack\services\src\saddr\ -I D:\ti\
    simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\
    ..\..\..\source\ti\ble5stack\services\src\sdata\ -I D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\
    ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\devices\cc26x0r2\ -I D:\ti\
    simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\
    ..\..\..\source\ -Ohz" --linkOptions "--no_out_extension -o D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\
    CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\FlashROM_StackLibrary\Exe\
    ble5_simple_peripheral_cc2640r2lp_app_FlashROM_StackLibrary.out --config_def CC2650=2 --config_def FLASH_ROM_BUILD=2 --map
    D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\
    FlashROM_StackLibrary\List\ble5_simple_peripheral_cc2640r2lp_app_FlashROM_StackLibrary.map --config D:\ti\
    simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\
    ..\..\..\source\ti\ble5stack\common\cc26xx\iar\cc26xx_app_and_stack.icf --keep __vector_table -f D:\ti\
    simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\config\
    configPkg\linker.cmd -f D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\
    tirtos\iar\app\..\config\lib_linker.cmd D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\
    simple_peripheral\tirtos\iar\app\..\config\ble_r2.symbols D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\
    CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\devices\cc26x0r2\driverlib\
    bin\iar\driverlib.lib D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\
    tirtos\iar\app\..\..\..\..\..\..\..\..\kernel\tirtos\packages\ti\dpl\lib\dpl_cc26x0r2.arm3 D:\ti\
    simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\
    ..\..\..\source\ti\drivers\lib\drivers_cc26x0r2.arm3 D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\
    CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\drivers\rf\lib\
    rf_singleMode_cc26x0r2.arm3 D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\display\lib\display.arm3 D:\ti\
    simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\
    ..\..\..\source\ti\grlib\lib\iar\m3\grlib.a --entry __iar_program_start --vfe --text_out locale" --profile release
    --projFile "D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\
    app\cc2640r2lp_app.ewp" --cfgArgs NO_ROM=0 -o D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\CC2640R2_LAUNCHXL\
    ble5stack\simple_peripheral\tirtos\iar\app\..\config\configPkg D:\ti\simplelink_cc2640r2_sdk_3_30_00_20\examples\rtos\
    CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\..\..\..\tirtos\app_ble.cfg

    Total number of errors: 1
    Total number of warnings: 0

  • Hi,

    1) Can you try using the recommended IAR version (IAR 8.32.2)?

    2) Do you have any global custom argvars defined? If so please disable them before you open the workspace.

  • Hi ,

    thank you reply, i already fix it.   remove iar path space, it's work fine.

  • Hi,

                  I have also face the same problem.

    from where to i should remove iar path space.

    and my build error is 

    Building configuration: cc2640r2lp_app - FlashROM_StackLibrary_RCOSC
    Updating build tree...

    0 file(s) deleted.
    Updating build tree...
    Performing Pre-Build Action
    Error while running "C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\..\xdctools_3_50_02_20_core\
    xs" --xdcpath="C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\kernel\tirtos\packages;C:\ti\
    simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source;C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\
    examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack" iar.tools.configuro -c "C:\Program Files (x86)\IAR Systems\Embedded
    Workbench 8.2\arm" --cc "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\bin\iccarm.exe" --device "CC2640R2F" --compileOptions "dummy.c -D
    BOARD_DISPLAY_USE_LCD=0 -D BOARD_DISPLAY_USE_UART=1 -D BOARD_DISPLAY_USE_UART_ANSI=1 -D CC2640R2_LAUNCHXL -D CC26XX -D CC26XX_R2 -D
    DeviceFamily_CC26X0R2 -D xDisplay_DISABLE_ALL -D ICALL_EVENTS -D ICALL_JT -D ICALL_LITE -D ICALL_MAX_NUM_ENTITIES=6 -D ICALL_MAX_NUM_TASKS=3 -D
    ICALL_STACK0_ADDR -D MAX_NUM_BLE_CONNS=1 -D POWER_SAVING -D STACK_LIBRARY -D USE_ICALL -D USE_RCOSC -D xdc_runtime_Assert_DISABLE_ALL -D
    xdc_runtime_Log_DISABLE_ALL --diag_suppress Pa050 -o C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\
    FlashROM_StackLibrary_RCOSC\Obj --debug --endian=little --cpu=Cortex-M3 -f C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\config\build_components.opt -f C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\
    blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\config\factory_config.opt -f C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\
    blestack\simple_peripheral\tirtos\iar\app\..\..\..\tirtos\build_config.opt -f C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\
    iar\app\..\config\configPkg\compiler.opt.defs -e --fpu=None --dlib_config \"C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\inc\c\DLib_Config_Normal.h\" -I C:\ti\
    simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\controller\cc26xx_r2\inc\ -I C:\ti\
    simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\inc\ -I C:\ti\
    simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\common\cc26xx\ -I C:\ti\
    simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\common\cc26xx\rcosc\ -I C:\ti\
    simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\src\app\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\
    examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\icall\inc\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\
    CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\inc\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\
    blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\profiles\dev_info\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\profiles\roles\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\profiles\roles\cc26xx\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\profiles\simple_profile\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\profiles\simple_profile\cc26xx\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\
    blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\target\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\hal\src\inc\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\hal\src\target\_common\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\hal\src\target\_common\cc26xx\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\
    blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\heapmgr\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\icall\src\inc\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\osal\src\inc\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\services\src\saddr\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\services\src\sdata\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\devices\cc26x0r2\ -I C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\
    tirtos\iar\app\..\..\..\..\..\..\..\..\source\ -Ohz" --linkOptions "--no_out_extension -o C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\
    simple_peripheral\tirtos\iar\app\FlashROM_StackLibrary_RCOSC\Exe\ble_simple_peripheral_cc2640r2lp_app_FlashROM_StackLibrary_RCOSC.out --config_def CC2650=2 --config_def
    FLASH_ROM_BUILD=2 --map C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\
    FlashROM_StackLibrary_RCOSC\List\ble_simple_peripheral_cc2640r2lp_app_FlashROM_StackLibrary_RCOSC.map --config C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\
    CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\blestack\common\cc26xx\iar\cc26xx_app_and_stack.icf --keep __vector_table -f C:\ti\
    simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\config\configPkg\linker.cmd -f C:\ti\
    simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\config\lib_linker.cmd C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\
    examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\config\ble_r2.symbols C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\
    CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\devices\cc26x0r2\driverlib\bin\iar\driverlib.lib C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\
    examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\kernel\tirtos\packages\ti\dpl\lib\dpl_cc26x0r2.arm3 C:\ti\
    simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\drivers\lib\drivers_cc26x0r2.arm3 C:\ti\
    simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\drivers\rf\lib\rf_singleMode_cc26x0r2.arm3
    C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\display\lib\display.arm3 C:\ti\
    simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\..\..\..\..\..\source\ti\grlib\lib\iar\m3\grlib.a --entry
    __iar_program_start --vfe --text_out locale" --profile release --projFile "C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\
    iar\app\cc2640r2lp_app.ewp" --cfgArgs NO_ROM=0 -o C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\
    config\configPkg C:\ti\simplelink_cc2640r2_sdk_3_10_00_15\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\..\..\tirtos\app_ble.cfg

    Total number of errors: 1
    Total number of warnings: 0

    i am using ID3E 8.32.2 ARM

    and SDK simplelink_cc2640r2_sdk_3_10_00_15

    XDC tool xdctools_3_50_02_20_core, xdctools_3_51_02_21_core

  • Hi Bhanu,

    make sure there is no blank space in your workspace name.