This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/CC2640R2F: LDO mode vs DC-DC converter mode

Part Number: CC2640R2F

Tool/software: WEBENCH® Design Tools

based on the application note below, they have mentioned DC-DC converter mode is the most power-efficient mode. 

https://www.ti.com/lit/an/swra640c/swra640c.pdf

in theory, 

"Switching regulators usually provide greater efficiency for applications, operating at higher power levels. This makes them ideal for line powered, low-power systems, which focus on increasing efficiency and reducing dynamic power consumption. Even so, they tend to have very low efficiency at low supply currents. A boost regulator, that can be 95% efficient at 50 mA, is likely to have efficiency around 20% or lower at a load current of 10 uA. Keep this in mind when designing a low-power system, which may spend most of its time asleep, as it can result in a linear regulator being a more efficient choice overall."

basically we have two type of power, dynamic power and static power. static power is when the MCU is supplied with power but not running any code. dynamic power is when the MCU running codes. based on theory, LDO will be suitable for power saving for battery-operated embedded systems that spend most of the time in static power state. 

please clarify if LDO mode is the best for static power state. 

  • Hi Pragash,

    The DCDC regulator is used dynamically to recharge a capacitor supplying the circuitry which is sleeping in Standby. This way the DCDC efficiency is leveraged also in Standby mode. This operation is tailored specifically for the CC13xx/CC26xx.

    In other words, the DCDC regulator is most efficient in any mode of operation for the CC2640R2F.

    Regards,
    Fredrik