Other Parts Discussed in Thread: BLE-STACK
Tool/software: WEBENCH® Design Tools
based on the datasheet,
"Bluetooth low energy requires a slow-speed clock with better than ±500 ppm accuracy if the device is to enter any sleep mode while maintaining a connection. The internal 32-kHz RC oscillator can in some use cases be compensated to meet the requirements. The low-speed crystal oscillator is designed for use with a 32-kHz watch-type crystal."
is that means MCU can be in shutdown mode but still initiate Bluetooth connection and establish the connection? based on the architecture, it looks like Main CPU, RF Core (Bluetooth), Peripherals and sensor controllers are separate modules inside this chip and can work independently of each other. correct me if I'm wrong.