This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/BOOSTXL-CC2650MA: Couldn't load the program into the BOOSTXL-CC2650MA.

Part Number: BOOSTXL-CC2650MA

Tool/software: Code Composer Studio

I tried to build and load the project of of CC2650bp .but it couldn't load the prgram. fail messages are: Cortex_M3_0: GEL Output: Memory Map Initialization Complete. Cortex_M3_0: GEL Output: Board Reset Complete. Cortex_M3_0: Command=20 -- addr=0x00001000 -- length=0x00001000 Cortex_M3_0: File Loader: Memory write failed: Timed out waiting for target flashloader to execute command. Cortex_M3_0: GEL: File: C:\ccs\workspace\simple_np_cc2650bp_app\FlashROM\simple_np_cc2650bp_app.out: Load failed. this project is importing following folder (C:\ti\simplelink\ble_sdk_2_02_03_08\examples\cc2650bp\simple_np\ccs). Please let me know the how to load nomaly. Best regards.