Hi,
I can not see explicitly in the release notes from simplelink_cc2640r2_sdk_3_30_00_20 any change regarding the maximum number of samples from a CTE.
When using simplelink_cc2640r2_sdk_3_20_00_21, sampling of a CTE with maximum length provided 32 chunks of 16 samples each, i.e 512 samples.
In simplelink_cc2640r2_sdk_3_30_00_20, the same setup will only provide 511 samples?
Is that change intentional?
Kind regards,
David