This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564MODA: Act as BT server (iSPP) + BLE client with multiple devices

Part Number: CC2564MODA

Hello, 

I actually have a programme running on a STM32F4 with a CC2564MODA using iSPP profile as server to communicate with a smartphone.
I want to add a feature to be able to get data from less than 10 BLE devices acting as server.
On example SPPLEDemo I saw that UI_Mode is a common variable for all the file. In my case I need to be BT Server and BLE client, I guess this example will not works fine for me.

My questions:
 1) Is it possible to be both BT Server and BLE client at same time ?
 2) if yes, shoud I use SPPLDemo at starting point or there is a more suitable programme to include BLE client feature ? If I need to use SPPLDemo, what should I do to adapt the program ? Need I to call "InitializeApplication" function 2 times ?
 3) what is the memory impact on the flash (estimation of BLE client size) ?

Thanks for yours advices.

Regards, 

Dam