Other Parts Discussed in Thread: CC2540
Hello,
I'm working with the BLE CC2540 development kit and running into a roadblock.
I've download the evaluation version of IAR 7.51A and then applied the patch to bring me up to EW8051-7.51L-EV. Whenever I load the SimpleBLEPeriferal project in IAR, it gives me 3 dialog alerts:
1) The project 'SimpleBLEPeripheral' contains the unknown tool 'CHIPCON_ID'
2) Invalid driver (/driver) option
3) An error occured trying to initialize the debugger. Debugging will not be available in this session.
'Make' works fine, but when I go to the project Options -> Debugger, the driver is blank and I have a blank subcategory under 'Debugger' called CHIPCON_ID.
Of course, if I try to hit the debugger icon, nothing happens. My hope is that hitting the debugger icon will send the compiled project to the keyfob connected through the hardware 'CC Debugger'.
Has anyone seen anything similar? Any help is appreciated.
Thanks,
Jon