This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352R: What is the time delay between the absolute trigger time and the actual frame transmission (from the beginning of the preamble)?

Part Number: CC1352R


Hi,

I work on LAUNCHXL-CC1352R1 (chip revision E).

I’m setting up an initial one-way time synchronization between two nodes.
I wonder, what is the time delay between the absolute trigger time of the frame and the actual transmission (from the beginning of the preamble)?

Based on the measurements I did, it seems to be around 90us of the time gap.
I have to take this constant value into account.

How can I calculate this delay time?

It has something to do with startToTXRatOffset and probably with the delay on the last power amplifier stage.

/Adam

  • Please explain how you are measuring this 90 us time gap (what do you use as an indication of the absolute trigger time?)

    Siri

  • Hi Siri

    Take a look at this answer:
    e2e.ti.com/.../646759

    > Please explain how you are measuring this 90 us time gap (what do you use as an indication of the absolute trigger time?)

    As I wrote in the original post.
    I’m setting up an initial one-way time synchronization between two nodes.
    This time gap is a difference between the same timeslots on the clock source and the clock receiver side just after one-way time synchronization.
    The time gap between timeslots is measured using an oscilloscope and the frame transmission is captured via routed PINs.
    PINCC26XX_setMux(pinHandle, IOID_5, PINCC26XX_MUX_RFC_GPO3); // GPO3 - high while transmitting
    No LBT procedure is used so the time error is deterministic.


    /Adam

  • Sorry, but I still have problems understanding what you are referring to when talking about "timeslots on the clock source" and the "clock receiver side".

    You are also not saying anything about how you are doing synchronization.

    It would help if you can provide some kind of figure/timing diagram where you show what you are doing in the code, and where you are measuring.

    It isn't even clear to me if the 90 us gap you are referring to is between a signal on the TX and a signal on the RX or between signals on the TX side.

    I also recommend that you take a look here and see if that answers any of your questions:

    Siri

  • Siri

    I think you missed the point.
    You are concentrating on the 90us time gap but the question in the post was clearly stated.
    Can we go back to the question?

    Question was:
    What is the time delay between the absolute trigger time and the actual frame transmission (from the beginning of the preamble)?
    I'm using CMD_IEEE_TX command.

    There is a magic parameter "startToTXRatOffset" mentioned once in the manual which probably is responsible for this time delay.

    Simply, I send frame using CMD_IEEE_TX command and absolute trigger time X. This particular command is sent 90-100us later than the scheduled time.
    Why is it so?
    How can I control this time gap value?
    Is this additional time present only in IEEE commands?
    Are other than IEEE commands send at a scheduled time?

    /Adam

  • I did additional tests.
    I send frame using:
    rfc_CMD_IEEE_TX_t TRONIX_cmdIeeeTx = {
             .commandNo = CMD_IEEE_TX,
             .startTrigger.triggerType = TRIG_NOW,
             .startTime = X
    };

    I read actual send time using:
    TRONIX_cmdIeeeTx.timeStamp

    Values are as follows:
    scheduled time: 19769705 timestamp: 19770089
    scheduled time: 23769705 timestamp: 23770089
    scheduled time: 27769707 timestamp: 27770091
    scheduled time: 31769707 timestamp: 31770091
    scheduled time: 35769706 timestamp: 35770090

    Assumptions:
    There is no LBT procedure.

    Conclusions:
    The frame is sent ~380 RATs (95us) later than the scheduled time.

    Why is it so?

    /Adam

  • Hi Adam

    I have been able to get some info from the modem team. startToTxRatOffset is the time from the start time programmed in the TX command to the trigger to the modem telling it to start TX. This time is default 96 us.

    Setting it too low will have the start happen as soon as possible (and how soon this is might vary) and you will no longer have full control of the start time.

    The override for adjusting this time is:

     ((startToTxRatOffset << 16) | 0x0203)

    BR

    Siri

  • Hi Siri

    Thank you for your assistance.
    This is the answer I was looking for.

    /Adam