Tool/software: Code Composer Studio
Hi,
I am using CC2642 and V3.2 SDK to develop AOA. Now I find that when the slave and passive is more than 1meter, the RSSI value is always near the same, about 0xa4~ 0xb9. when I move the slave to even 5 meter away or even farther, the value is still this area. I think maybe the tx power is to small. so I check the TX power of slave , as following
.txPower = GAP_ADV_TX_POWER_NO_PREFERENCE (127)
I also try to change the value to 10, but the RSSI area is the same. I am not sure whether the RSSI area is normal or not. if the Tx power matters ,how to change it? and if not, what else can I do? thank you
best regards
Yanpo, Li