This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bluetooth Solution Recommendation

Other Parts Discussed in Thread: CC2564

I have a customer requesting a Bluetooth solution recommendation with requirements that push me out of my comfort zone, hence looking for more expert input. The requirements are for a portable headset-like device, and include running the A2DP and HSP profiles streaming music and phone call audio to the headset from a phone, while simultaneously using the SPP profile to stream up to 200Kbps of data from the device back to the phone. I believe these requirements may be challenging at a minimum. Can you advise whether any BT solution TI or your partners offer could meet these requirements? Thanks!

  • For such bluetooth application, the choice of TI chip is CC2564. There is no data that shows CC2564 can do the A2DP and HSP profiles streaming music and phone call audio to the headset from a phone, while simultaneously using the SPP profile to stream up to 200Kbps of data from the device back to the phone so you might need to test to know if it works.