This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541: I have a question about CC2541

Part Number: CC2541

Hi.


I'm making a customized BLE module using CC2541 that is compatible with Arduino.

I organized the circuit except for the antenna part(pin26, 26) with the newly purchased CC2541 (XTAL1 - 32M; XTAL2 - 32.768K; C221, C232 - 12pF; C331, C321 -15pF; C401 - 1uF; R301 - 56K;)

And then, I updated the firmware for the HM10 by following the link at https://forum.arduino.cc/index.php?topic=393655.0


I succeeded in updating the firmware but received no response when I sent AT command.

I think the response to the AT should come even without the antenna part, but I wonder if it's wrong.

If it's wrong, I wonder what is the problem.

I also have a CC debugger and I want to know how to use it. I have already checked and followed the User Guide but can not get the results I wanted.

The content is difficult, so I need advice from someone with similar experience.

Thank you