Part Number: CC2642R
Other Parts Discussed in Thread: LAUNCHXL-CC26X2R1,
Tool/software: Code Composer Studio
Hi,
I am working on BLE project using CC2642r controller and we made a custom board for the project, planning to run the controller on 2.8v. After soldering the controller and it's basic circuitry programmed controller using the LAUNCHXL-CC26X2R1 for numerous times(power given through development board) and it worked fine. After adding the 2.8v regulator tried loading the code to controller but now IDE started giving me "error IcePick_C: Error connecting to the target: (Error -242 @ 0x0) A router subpath could not be accessed. The board configuration file is probably incorrect. (Emulation package 8.1.0.00007)". I removed regulator and given power through the development board still IDE is throwing me the same error. As my test code is already loaded in to the controller I believe it should start advertising once I give power to controller but it is not advertising most of the times but some times it does advertising. I am clueless about this issue please help me if anybody knows the solution for this issue.
And one more doubt is it necessary to solder ground pad of the controller to ground? However I soldered it to ground.
My CCS Version: 9.0.1.00004 and sdk version 3.10.00.53.