Part Number: CC2642R
What is the maximum length of data which can be transmitted in a single connection interval. I have set the MAX_PDU_SIZE macro as 255. My connection interval is set at 7.5 ms. I believe I have all the values to be the maximum permissible - as per the TI forums.
So this means that the maximum BLE throughput that can be achieved with this configuration is 272,000 bits per second(255 Bytes every 7.5 ms). But this contradicts the maximum throughput for BLE as per the spec, the BLE spec states that BLE throughput of 2M bits per second can be achieved with BLE 5. Is there a way to improve my BLE throughput??