This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564MODA: HCITester issues

Part Number: CC2564MODA

Hi,

My customer has troubles using HCITester with CC2564B.

Software environments:
HCITester version 3.0.0.37
ServicePack CC256XB_BT_SP v1.8

Customer refers below document:
http://www.ti.com/lit/ml/swru136b/swru136b.pdf

PC and the target is connected with FTDI cable.
Serial port is configured as Three Wire:


Customer also tried Hardware Flow control, but results are the same.


Here are some steps customer did:
1) Change XML file(command library) to TIInit_6.7.16.xml which comes with CC256XB_BT_SP.
2) Open BTS file(initscripts-TIInit_6.7.16_bt_spec_4.1.bts)
3) Copy BTS file and replace all “5000, 0x00” with “5000, any” (as described in section 3.2 in swru136.pdf)
4) Execute the script

Issues
1) As soon as the script is executed. Script parse error is generated at line#1.
#--------------------------------------------------------------------------------   <== here
It seems the ‘#’ is not recognized as “comment line”.
If another “#” is added at the beginning of the line, the error is gone. Why?

2) After the error 1) is removed, the 1st command (changing UART baudrate) always fails with timeout

14:58:20.430 ERROR - Timeout waiting for event HCI_Command_Complete_VS_Update_Uart_HCI_Baudrate_Event

14:58:20.430 ERRORed Line (9): Wait_HCI_Command_Complete_VS_Update_Uart_HCI_Baudrate_Event 5000, any, 0xff36, 0x00

14:58:20.430 --

14:58:20.430 *** Script End ***

14:58:20.430 --


Could you tell me what goes wrong?

Thanks and regards,
Koichiro Tashiro