This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564: Advertisement is not started although hci command succeeded

Part Number: CC2564

Hallo,

we have encountered a similar problem to:

https://e2e.ti.com/support/wireless-connectivity/bluetooth/f/538/t/615843?CC2564-advertising-stops-after-1-or-2-days

The ble module stops advertising although advertisement was started and acknowledged. HCI Log:

Frame 137826: 5 bytes on wire (40 bits), 5 bytes captured (40 bits)
Bluetooth
PacketLogger HCI Command
Type: HCI Command (0x00)
Bluetooth HCI Command - LE Set Advertise Enable
Command Opcode: LE Set Advertise Enable (0x200a)
Parameter Total Length: 1
Advertising Enable: true (0x01)
[Response in frame: 137828]
[Command-Response Delta: 1.679ms]

No. Time Source Destination Protocol Length Info
137828 13459298.857274 controller host HCI_EVT 7 Rcvd Command Complete (LE Set Advertise Enable)

Frame 137828: 7 bytes on wire (56 bits), 7 bytes captured (56 bits)
Bluetooth
PacketLogger HCI Event
Type: HCI Event (0x01)
Bluetooth HCI Event - Command Complete
Event Code: Command Complete (0x0e)
Parameter Total Length: 4
Number of Allowed Command Packets: 1
Command Opcode: LE Set Advertise Enable (0x200a)
Status: Success (0x00)
[Command in frame: 137826]
[Command-Response Delta: 1.679ms]

Could you please give some information how the original problem was solved or how to proceed in our case.

Greetings