Part Number: CC2640R2F
Tool/software: Code Composer Studio
Hello.
I have a problem.
I am working with HM-16 and HM-17 which have cc2640r2f.
(I connected TCK, TMS, VCC, GND, Reset)
I have an XDS110 debugger.
I work with CCS v.9 and flash programmer 2.
My project is Simple Peripheral.
My problem in flash programmer 2 is that
I can force mass erase the first part successfully.
But the second part:
>Initiate access to target: COM9 using 2-pin cJTAG.
>ACK/NAK not received. Expected 0x00 0xCC or 0x00 0x33, received 0x00 0x00.
>ACK/NAK not received. Expected 0x00 0xCC or 0x00 0x33, received 0x00 0x00.
>No response from device. Device may not be in bootloader mode. Reset device and try again.
If problem persists, check connection and baud rate.
>Connecting over serial bootloader failed: No response from device. Device may not be in bootloader mode. Reset device and try again.
If problem persists, check connection and baud rate.
>Failed to create device object.
And when I try to debug the program in CCS, I receive error 242 which is : A router subpath could not be accessed. The board configuration file is probably incorrect.
How can I solve this?