This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: Boot up power sequence timing requirement....

Part Number: CC2642R
Other Parts Discussed in Thread: BQ24230

Dear sir:

   Our system is wearable device base on the CC2642R. When the battery run out of power, I plug the power adapter to boot our system.

   But the CC2642R boot failed. I check the charging IC (BQ24230), this output voltage is 4.4V and it can charge our battery..

   Normally our system work fine when used only battery  or plug power adapter...

   Does the CC2642R need to meet boot up power sequence requirement or you have other suggestions for me...

Best Regards

Ting  2020/01/17