This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650MODA: Real time BLE application

Part Number: CC2650MODA
Other Parts Discussed in Thread: CC2640R2F

Hello everyone,

I'm developing a device with 4 gyroscopes. The idea is to send each IMU data to a smartphone using Bluetooth and visualizate in it in "real time". As the device has to have a battery, in a beginning I thought to send the data with BLE using CC2650MODA but now I have doubts due to the data rate. I would like to send 4 short strings (each one with the data of each gyroscope) each 100 ms or even less.

Do you think is possible to get that data rate using CC2650MODA based on Simple_peripheral application? 

How often could I send data?

Thank you very much!

Jorge