Hello,
I was working with the LPSTK-CC1352 board and ran into an issue after using the over the air download to change the program. I was using the Ti app on my phone and used the FW Download tab and changed it from the out of the box code. It did the firmware update and changed it to the other project zero that was available on the selection screen. The problem is, I can no longer get sensor readings from the app and I am not able to "Restore to the factory image" as stated in the simple link academy for this board. Is there a different way to reset the board so that I can get it back to how it was out of the box?
Thank you,
Abel Martinez