This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640R2F: Problem ADC GPIO Config

Part Number: CC2640R2F
Other Parts Discussed in Thread: SYSCONFIG

Tool/software: Code Composer Studio

Hi,

I'm having the same problem already described in another topic.

When configuring the ADC the value read is always the same.

The hardware is functioning properly.

I tested on more than 1 processor pin and the same occurred.

It is clearly a pin configuration error. The problem is that the previous topic was closed without making it clear what the error was and what was changed.

So what is the gpio error that causes this problem?

Another question. Why does cc2640r2 empty_project not have syscfg like cc26x2?

void *TaskButtonADC(void *arg0)
{
ADC_Handle adc_handle;
ADC_Params params;
uint16_t adcValue;

ADC_Params_init(&params);
adc_handle = ADC_open(Board_ADC0, &params);
while (1) {
if (ADC_convert(adc_handle, &adcValue) == ADC_STATUS_SUCCESS) {
if(adcValue == 0){

}else if(adcValue == 1){

}else if(adcValue == 2){

}
}
sleep(1);
}
}

4251.CC2640R2_LAUNCHXL.h

/*
 * Copyright (c) 2016-2019, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

/*
 *  ====================== CC2640R2_LAUNCHXL.c ===================================
 *  This file is responsible for setting up the board specific items for the
 *  CC2640R2_LAUNCHXL board.
 */

#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>

#include <ti/devices/cc26x0r2/driverlib/ioc.h>
#include <ti/devices/cc26x0r2/driverlib/udma.h>
#include <ti/devices/cc26x0r2/inc/hw_ints.h>
#include <ti/devices/cc26x0r2/inc/hw_memmap.h>

#include "CC2640R2_LAUNCHXL.h"

/*
 *  =============================== ADCBuf ===============================
 */
//#include <ti/drivers/ADCBuf.h>
//#include <ti/drivers/adcbuf/ADCBufCC26XX.h>

//ADCBufCC26XX_Object adcBufCC26xxObjects[CC2640R2_LAUNCHXL_ADCBUFCOUNT];

/*
 *  This table converts a virtual adc channel into a dio and internal analogue
 *  input signal. This table is necessary for the functioning of the adcBuf
 *  driver. Comment out unused entries to save flash. Dio and internal signal
 *  pairs are hardwired. Do not remap them in the table. You may reorder entire
 *  entries. The mapping of dio and internal signals is package dependent.
 */
/*
const ADCBufCC26XX_AdcChannelLutEntry ADCBufCC26XX_adcChannelLut[CC2640R2_LAUNCHXL_ADCBUF0CHANNELCOUNT] = {
    {CC2640R2_LAUNCHXL_DIO23_ANALOG, ADC_COMPB_IN_AUXIO7},
    {CC2640R2_LAUNCHXL_DIO24_ANALOG, ADC_COMPB_IN_AUXIO6},
    {CC2640R2_LAUNCHXL_DIO25_ANALOG, ADC_COMPB_IN_AUXIO5},
    {CC2640R2_LAUNCHXL_DIO26_ANALOG, ADC_COMPB_IN_AUXIO4},
    {CC2640R2_LAUNCHXL_DIO27_ANALOG, ADC_COMPB_IN_AUXIO3},
    {CC2640R2_LAUNCHXL_DIO28_ANALOG, ADC_COMPB_IN_AUXIO2},
    {CC2640R2_LAUNCHXL_DIO29_ANALOG, ADC_COMPB_IN_AUXIO1},
    {CC2640R2_LAUNCHXL_DIO30_ANALOG, ADC_COMPB_IN_AUXIO0},
    {PIN_UNASSIGNED, ADC_COMPB_IN_VDDS},
    {PIN_UNASSIGNED, ADC_COMPB_IN_DCOUPL},
    {PIN_UNASSIGNED, ADC_COMPB_IN_VSS},
};

const ADCBufCC26XX_HWAttrs adcBufCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADCBUFCOUNT] = {
    {
        .intPriority       = ~0,
        .swiPriority       = 0,
        .adcChannelLut     = ADCBufCC26XX_adcChannelLut,
    }
};

const ADCBuf_Config ADCBuf_config[CC2640R2_LAUNCHXL_ADCBUFCOUNT] = {
    {
        &ADCBufCC26XX_fxnTable,
        &adcBufCC26xxObjects[CC2640R2_LAUNCHXL_ADCBUF0],
        &adcBufCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADCBUF0]
    },
};

const uint_least8_t ADCBuf_count = CC2640R2_LAUNCHXL_ADCBUFCOUNT;
*/
/*
 *  =============================== ADC ===============================
 */
#include <ti/drivers/ADC.h>
#include <ti/drivers/adc/ADCCC26XX.h>

ADCCC26XX_Object adcCC26xxObjects[CC2640R2_LAUNCHXL_ADCCOUNT];

const ADCCC26XX_HWAttrs adcCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADCCOUNT] = {
    {
        .adcDIO              = CC2640R2_LAUNCHXL_DIO23_ANALOG,
        .adcCompBInput       = ADC_COMPB_IN_VDDS,
        .refSource           = ADCCC26XX_FIXED_REFERENCE,
        .samplingDuration    = ADCCC26XX_SAMPLING_DURATION_2P7_US,
        .inputScalingEnabled = false,
        .triggerSource       = ADCCC26XX_TRIGGER_MANUAL,
        .returnAdjustedVal   = false
    },
    {
        .adcDIO              = CC2640R2_LAUNCHXL_DIO24_ANALOG,
        .adcCompBInput       = ADC_COMPB_IN_VDDS,
        .refSource           = ADCCC26XX_FIXED_REFERENCE,
        .samplingDuration    = ADCCC26XX_SAMPLING_DURATION_2P7_US,
        .inputScalingEnabled = false,
        .triggerSource       = ADCCC26XX_TRIGGER_MANUAL,
        .returnAdjustedVal   = false
    }/*,
    {
        .adcDIO              = PIN_UNASSIGNED,
        .adcCompBInput       = ADC_COMPB_IN_AUXIO5,
        .refSource           = ADCCC26XX_FIXED_REFERENCE,
        .samplingDuration    = ADCCC26XX_SAMPLING_DURATION_2P7_US,
        .inputScalingEnabled = true,
        .triggerSource       = ADCCC26XX_TRIGGER_MANUAL,
        .returnAdjustedVal   = false
    },
    {
        .adcDIO              = PIN_UNASSIGNED,
        .adcCompBInput       = ADC_COMPB_IN_AUXIO4,
        .refSource           = ADCCC26XX_FIXED_REFERENCE,
        .samplingDuration    = ADCCC26XX_SAMPLING_DURATION_2P7_US,
        .inputScalingEnabled = true,
        .triggerSource       = ADCCC26XX_TRIGGER_MANUAL,
        .returnAdjustedVal   = false
    },
    {
        .adcDIO              = PIN_UNASSIGNED,
        .adcCompBInput       = ADC_COMPB_IN_AUXIO3,
        .refSource           = ADCCC26XX_FIXED_REFERENCE,
        .samplingDuration    = ADCCC26XX_SAMPLING_DURATION_2P7_US,
        .inputScalingEnabled = true,
        .triggerSource       = ADCCC26XX_TRIGGER_MANUAL,
        .returnAdjustedVal   = false
    },
    {
        .adcDIO              = PIN_UNASSIGNED,
        .adcCompBInput       = ADC_COMPB_IN_AUXIO2,
        .refSource           = ADCCC26XX_FIXED_REFERENCE,
        .samplingDuration    = ADCCC26XX_SAMPLING_DURATION_2P7_US,
        .inputScalingEnabled = true,
        .triggerSource       = ADCCC26XX_TRIGGER_MANUAL,
        .returnAdjustedVal   = false
    },
    {
        .adcDIO              = PIN_UNASSIGNED,
        .adcCompBInput       = ADC_COMPB_IN_AUXIO1,
        .refSource           = ADCCC26XX_FIXED_REFERENCE,
        .samplingDuration    = ADCCC26XX_SAMPLING_DURATION_2P7_US,
        .inputScalingEnabled = true,
        .triggerSource       = ADCCC26XX_TRIGGER_MANUAL,
        .returnAdjustedVal   = false
    },
    {
        .adcDIO              = PIN_UNASSIGNED,
        .adcCompBInput       = ADC_COMPB_IN_AUXIO0,
        .refSource           = ADCCC26XX_FIXED_REFERENCE,
        .samplingDuration    = ADCCC26XX_SAMPLING_DURATION_10P9_MS,
        .inputScalingEnabled = true,
        .triggerSource       = ADCCC26XX_TRIGGER_MANUAL,
        .returnAdjustedVal   = false
    },
    {
        .adcDIO              = PIN_UNASSIGNED,
        .adcCompBInput       = ADC_COMPB_IN_DCOUPL,
        .refSource           = ADCCC26XX_FIXED_REFERENCE,
        .samplingDuration    = ADCCC26XX_SAMPLING_DURATION_2P7_US,
        .inputScalingEnabled = true,
        .triggerSource       = ADCCC26XX_TRIGGER_MANUAL,
        .returnAdjustedVal   = false
    },
    {
        .adcDIO              = PIN_UNASSIGNED,
        .adcCompBInput       = ADC_COMPB_IN_VSS,
        .refSource           = ADCCC26XX_FIXED_REFERENCE,
        .samplingDuration    = ADCCC26XX_SAMPLING_DURATION_2P7_US,
        .inputScalingEnabled = true,
        .triggerSource       = ADCCC26XX_TRIGGER_MANUAL,
        .returnAdjustedVal   = false
    },
    {
        .adcDIO              = PIN_UNASSIGNED,
        .adcCompBInput       = ADC_COMPB_IN_VDDS,
        .refSource           = ADCCC26XX_FIXED_REFERENCE,
        .samplingDuration    = ADCCC26XX_SAMPLING_DURATION_2P7_US,
        .inputScalingEnabled = true,
        .triggerSource       = ADCCC26XX_TRIGGER_MANUAL,
        .returnAdjustedVal   = false
    }*/
};

const ADC_Config ADC_config[CC2640R2_LAUNCHXL_ADCCOUNT] = {
    {&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC2640R2_LAUNCHXL_ADC0], &adcCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADC0]},
    {&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC2640R2_LAUNCHXL_ADC1], &adcCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADC1]}/*,
    {&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC2640R2_LAUNCHXL_ADC2], &adcCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADC2]},
    {&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC2640R2_LAUNCHXL_ADC3], &adcCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADC3]},
    {&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC2640R2_LAUNCHXL_ADC4], &adcCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADC4]},
    {&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC2640R2_LAUNCHXL_ADC5], &adcCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADC5]},
    {&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC2640R2_LAUNCHXL_ADC6], &adcCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADC6]},
    {&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC2640R2_LAUNCHXL_ADC7], &adcCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADC7]},
    {&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC2640R2_LAUNCHXL_ADCDCOUPL], &adcCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADCDCOUPL]},
    {&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC2640R2_LAUNCHXL_ADCVSS], &adcCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADCVSS]},
    {&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC2640R2_LAUNCHXL_ADCVDDS], &adcCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADCVDDS]},*/
};

const uint_least8_t ADC_count = CC2640R2_LAUNCHXL_ADCCOUNT;

/*
 *  =============================== Crypto ===============================
 */
#include <ti/drivers/crypto/CryptoCC26XX.h>

CryptoCC26XX_Object cryptoCC26XXObjects[CC2640R2_LAUNCHXL_CRYPTOCOUNT];

const CryptoCC26XX_HWAttrs cryptoCC26XXHWAttrs[CC2640R2_LAUNCHXL_CRYPTOCOUNT] = {
    {
        .baseAddr       = CRYPTO_BASE,
        .powerMngrId    = PowerCC26XX_PERIPH_CRYPTO,
        .intNum         = INT_CRYPTO_RESULT_AVAIL_IRQ,
        .intPriority    = ~0,
    }
};

const CryptoCC26XX_Config CryptoCC26XX_config[CC2640R2_LAUNCHXL_CRYPTOCOUNT] = {
    {
         .object  = &cryptoCC26XXObjects[CC2640R2_LAUNCHXL_CRYPTO0],
         .hwAttrs = &cryptoCC26XXHWAttrs[CC2640R2_LAUNCHXL_CRYPTO0]
    },
};

/*
 *  =============================== AESCCM ===============================
 */
/*#include <ti/drivers/AESCCM.h>
#include <ti/drivers/aesccm/AESCCMCC26XX.h>

AESCCMCC26XX_Object aesccmCC26XXObjects[CC2640R2_LAUNCHXL_AESCCMCOUNT];

const AESCCMCC26XX_HWAttrs aesccmCC26XXHWAttrs[CC2640R2_LAUNCHXL_AESCCMCOUNT] = {
    {
        .intPriority       = ~0,
    }
};

const AESCCM_Config AESCCM_config[CC2640R2_LAUNCHXL_AESCCMCOUNT] = {
    {
         .object  = &aesccmCC26XXObjects[CC2640R2_LAUNCHXL_AESCCM0],
         .hwAttrs = &aesccmCC26XXHWAttrs[CC2640R2_LAUNCHXL_AESCCM0]
    },
};

const uint_least8_t AESCCM_count = CC2640R2_LAUNCHXL_AESCCMCOUNT;


/*
 *  =============================== AESGCM ===============================
 */
/*#include <ti/drivers/AESGCM.h>
#include <ti/drivers/aesgcm/AESGCMCC26XX.h>

AESGCMCC26XX_Object aesgcmCC26XXObjects[CC2640R2_LAUNCHXL_AESGCMCOUNT];

const AESGCMCC26XX_HWAttrs aesgcmCC26XXHWAttrs[CC2640R2_LAUNCHXL_AESGCMCOUNT] = {
    {
        .intPriority       = ~0,
    }
};

const AESGCM_Config AESGCM_config[CC2640R2_LAUNCHXL_AESGCMCOUNT] = {
    {
         .object  = &aesgcmCC26XXObjects[CC2640R2_LAUNCHXL_AESGCM0],
         .hwAttrs = &aesgcmCC26XXHWAttrs[CC2640R2_LAUNCHXL_AESGCM0]
    },
};

const uint_least8_t AESGCM_count = CC2640R2_LAUNCHXL_AESGCMCOUNT;

/*
 *  =============================== AESCBC ===============================
 */
/*#include <ti/drivers/AESCBC.h>
#include <ti/drivers/aescbc/AESCBCCC26XX.h>

AESCBCCC26XX_Object aescbcCC26XXObjects[CC2640R2_LAUNCHXL_AESCBCCOUNT];

const AESCBCCC26XX_HWAttrs aescbcCC26XXHWAttrs[CC2640R2_LAUNCHXL_AESCBCCOUNT] = {
    {
        .intPriority       = ~0,
    }
};

const AESCBC_Config AESCBC_config[CC2640R2_LAUNCHXL_AESCBCCOUNT] = {
    {
         .object  = &aescbcCC26XXObjects[CC2640R2_LAUNCHXL_AESCBC0],
         .hwAttrs = &aescbcCC26XXHWAttrs[CC2640R2_LAUNCHXL_AESCBC0]
    },
};

const uint_least8_t AESCBC_count = CC2640R2_LAUNCHXL_AESCBCCOUNT;

/*
 *  =============================== AESCTR ===============================
 */
/*#include <ti/drivers/AESCTR.h>
#include <ti/drivers/aesctr/AESCTRCC26XX.h>

AESCTRCC26XX_Object aesctrCC26XXObjects[CC2640R2_LAUNCHXL_AESCTRCOUNT];

const AESCTRCC26XX_HWAttrs aesctrCC26XXHWAttrs[CC2640R2_LAUNCHXL_AESCTRCOUNT] = {
    {
        .intPriority       = ~0,
    }
};

const AESCTR_Config AESCTR_config[CC2640R2_LAUNCHXL_AESCTRCOUNT] = {
    {
         .object  = &aesctrCC26XXObjects[CC2640R2_LAUNCHXL_AESCTR0],
         .hwAttrs = &aesctrCC26XXHWAttrs[CC2640R2_LAUNCHXL_AESCTR0]
    },
};

const uint_least8_t AESCTR_count = CC2640R2_LAUNCHXL_AESCTRCOUNT;

/*
 *  =============================== AESECB ===============================
 */
/*#include <ti/drivers/AESECB.h>
#include <ti/drivers/aesecb/AESECBCC26XX.h>

AESECBCC26XX_Object aesecbCC26XXObjects[CC2640R2_LAUNCHXL_AESECBCOUNT];

const AESECBCC26XX_HWAttrs aesecbCC26XXHWAttrs[CC2640R2_LAUNCHXL_AESECBCOUNT] = {
    {
        .intPriority       = ~0,
    }
};

const AESECB_Config AESECB_config[CC2640R2_LAUNCHXL_AESECBCOUNT] = {
    {
         .object  = &aesecbCC26XXObjects[CC2640R2_LAUNCHXL_AESECB0],
         .hwAttrs = &aesecbCC26XXHWAttrs[CC2640R2_LAUNCHXL_AESECB0]
    },
};

const uint_least8_t AESECB_count = CC2640R2_LAUNCHXL_AESECBCOUNT;

/*
 *  =============================== AESCTRDRBG ===============================
 */
/*#include <ti/drivers/AESCTRDRBG.h>
#include <ti/drivers/aesctrdrbg/AESCTRDRBGXX.h>

AESCTRDRBGXX_Object aesctrdrbgXXObjects[CC2640R2_LAUNCHXL_AESCTRDRBGCOUNT];

const AESCTRDRBGXX_HWAttrs aesctrdrbgXXHWAttrs[CC2640R2_LAUNCHXL_AESCTRDRBGCOUNT] = {
    {
        .aesctrIndex       = CC2640R2_LAUNCHXL_AESCTR0,
    }
};

const AESCTRDRBG_Config AESCTRDRBG_config[CC2640R2_LAUNCHXL_AESCTRDRBGCOUNT] = {
    {
         .object  = &aesctrdrbgXXObjects[CC2640R2_LAUNCHXL_AESCTRDRBG0],
         .hwAttrs = &aesctrdrbgXXHWAttrs[CC2640R2_LAUNCHXL_AESCTRDRBG0]
    },
};

const uint_least8_t AESCTRDRBG_count = CC2640R2_LAUNCHXL_AESCTRDRBGCOUNT;

/*
 *  =============================== TRNG ===============================
 */
/*#include <ti/drivers/TRNG.h>
#include <ti/drivers/trng/TRNGCC26XX.h>

TRNGCC26XX_Object trngCC26XXObjects[CC2640R2_LAUNCHXL_TRNGCOUNT];

const TRNGCC26XX_HWAttrs trngCC26X2HWAttrs[CC2640R2_LAUNCHXL_TRNGCOUNT] = {
    {
        .intPriority       = ~0,
        .swiPriority       = 0,
        .samplesPerCycle   = 240000,
    }
};

const TRNG_Config TRNG_config[CC2640R2_LAUNCHXL_TRNGCOUNT] = {
    {
         .object  = &trngCC26XXObjects[CC2640R2_LAUNCHXL_TRNG0],
         .hwAttrs = &trngCC26X2HWAttrs[CC2640R2_LAUNCHXL_TRNG0]
    },
};

const uint_least8_t TRNG_count = CC2640R2_LAUNCHXL_TRNGCOUNT;


/*
 *  =============================== Display ===============================
 */
/*#include <ti/display/Display.h>
#include <ti/display/DisplayUart.h>
#include <ti/display/DisplaySharp.h>

#ifndef BOARD_DISPLAY_UART_STRBUF_SIZE
#define BOARD_DISPLAY_UART_STRBUF_SIZE    128
#endif

/* This value can be changed to 96 for use with the 430BOOST-SHARP96 BoosterPack. */
/*#define BOARD_DISPLAY_SHARP_SIZE    128

DisplayUart_Object     displayUartObject;
DisplaySharp_Object    displaySharpObject;

static char uartStringBuf[BOARD_DISPLAY_UART_STRBUF_SIZE];
static uint_least8_t sharpDisplayBuf[BOARD_DISPLAY_SHARP_SIZE * BOARD_DISPLAY_SHARP_SIZE / 8];

const DisplayUart_HWAttrs displayUartHWAttrs = {
    .uartIdx      = CC2640R2_LAUNCHXL_UART0,
    .baudRate     = 115200,
    .mutexTimeout = (unsigned int)(-1),
    .strBuf       = uartStringBuf,
    .strBufLen    = BOARD_DISPLAY_UART_STRBUF_SIZE,
};

const DisplaySharp_HWAttrsV1 displaySharpHWattrs = {
    .spiIndex    = CC2640R2_LAUNCHXL_SPI0,
    .csPin       = CC2640R2_LAUNCHXL_GPIO_LCD_CS,
    .powerPin    = CC2640R2_LAUNCHXL_GPIO_LCD_POWER,
    .enablePin   = CC2640R2_LAUNCHXL_GPIO_LCD_ENABLE,
    .pixelWidth  = BOARD_DISPLAY_SHARP_SIZE,
    .pixelHeight = BOARD_DISPLAY_SHARP_SIZE,
    .displayBuf  = sharpDisplayBuf,
};

#ifndef BOARD_DISPLAY_USE_UART
#define BOARD_DISPLAY_USE_UART 1
#endif
#ifndef BOARD_DISPLAY_USE_UART_ANSI
#define BOARD_DISPLAY_USE_UART_ANSI 0
#endif
#ifndef BOARD_DISPLAY_USE_LCD
#define BOARD_DISPLAY_USE_LCD 0
#endif

/*
 * This #if/#else is needed to workaround a problem with the
 * IAR compiler. The IAR compiler doesn't like the empty array
 * initialization. (IAR Error[Pe1345])
 */
/*#if (BOARD_DISPLAY_USE_UART || BOARD_DISPLAY_USE_LCD)

const Display_Config Display_config[] = {
#if (BOARD_DISPLAY_USE_UART)
    {
#  if (BOARD_DISPLAY_USE_UART_ANSI)
        .fxnTablePtr = &DisplayUartAnsi_fxnTable,
#  else /* Default to minimal UART with no cursor placement */
 /*       .fxnTablePtr = &DisplayUartMin_fxnTable,
#  endif
        .object      = &displayUartObject,
        .hwAttrs     = &displayUartHWAttrs,
    },
#endif
#if (BOARD_DISPLAY_USE_LCD)
    {
        .fxnTablePtr = &DisplaySharp_fxnTable,
        .object      = &displaySharpObject,
        .hwAttrs     = &displaySharpHWattrs
    },
#endif
};

const uint_least8_t Display_count = sizeof(Display_config) / sizeof(Display_Config);

#else

const Display_Config *Display_config = NULL;
const uint_least8_t Display_count = 0;

#endif /* (BOARD_DISPLAY_USE_UART || BOARD_DISPLAY_USE_LCD) */

/*
 *  =============================== GPIO ===============================
 */
#include <ti/drivers/GPIO.h>
#include <ti/drivers/gpio/GPIOCC26XX.h>

/*
 * Array of Pin configurations
 * NOTE: The order of the pin configurations must coincide with what was
 *       defined in CC2640R2_LAUNCHXL.h
 * NOTE: Pins not used for interrupts should be placed at the end of the
 *       array. Callback entries can be omitted from callbacks array to
 *       reduce memory usage.
 */
GPIO_PinConfig gpioPinConfigs[] = {
    GPIOCC26XX_DIO_00 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_01 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_02 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_03 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_04 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_05 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_06 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_07 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_08 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_09 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_10 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_11 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_12 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_13 | GPIO_DO_NOT_CONFIG,
    GPIOCC26XX_DIO_14 | GPIO_DO_NOT_CONFIG
};

/*
 * Array of callback function pointers
 * NOTE: The order of the pin configurations must coincide with what was
 *       defined in CC2640R2_LAUNCH.h
 * NOTE: Pins not used for interrupts can be omitted from callbacks array to
 *       reduce memory usage (if placed at end of gpioPinConfigs array).
 */
GPIO_CallbackFxn gpioCallbackFunctions[] = {
    NULL,  /* Button 0 */
    NULL,  /* Button 1 */
    NULL,  /* CC2640R2_LAUNCHXL_SPI_MASTER_READY */
    NULL,  /* CC2640R2_LAUNCHXL_SPI_SLAVE_READY */
};

const GPIOCC26XX_Config GPIOCC26XX_config = {
    .pinConfigs         = (GPIO_PinConfig *)gpioPinConfigs,
    .callbacks          = (GPIO_CallbackFxn *)gpioCallbackFunctions,
    .numberOfPinConfigs = CC2640R2_LAUNCHXL_GPIOCOUNT,
    .numberOfCallbacks  = sizeof(gpioCallbackFunctions)/sizeof(GPIO_CallbackFxn),
    .intPriority        = (~0)
};

/*
 *  =============================== GPTimer ===============================
 *  Remove unused entries to reduce flash usage both in Board.c and Board.h
 */
#include <ti/drivers/timer/GPTimerCC26XX.h>

GPTimerCC26XX_Object gptimerCC26XXObjects[CC2640R2_LAUNCHXL_GPTIMERCOUNT];

const GPTimerCC26XX_HWAttrs gptimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_GPTIMERPARTSCOUNT] = {
    { .baseAddr = GPT0_BASE, .intNum = INT_GPT0A, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT0, .pinMux = GPT_PIN_0A, },
    { .baseAddr = GPT0_BASE, .intNum = INT_GPT0B, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT0, .pinMux = GPT_PIN_0B, },
    { .baseAddr = GPT1_BASE, .intNum = INT_GPT1A, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT1, .pinMux = GPT_PIN_1A, },
    { .baseAddr = GPT1_BASE, .intNum = INT_GPT1B, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT1, .pinMux = GPT_PIN_1B, },
    { .baseAddr = GPT2_BASE, .intNum = INT_GPT2A, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT2, .pinMux = GPT_PIN_2A, },
    { .baseAddr = GPT2_BASE, .intNum = INT_GPT2B, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT2, .pinMux = GPT_PIN_2B, },
    { .baseAddr = GPT3_BASE, .intNum = INT_GPT3A, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT3, .pinMux = GPT_PIN_3A, },
    { .baseAddr = GPT3_BASE, .intNum = INT_GPT3B, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT3, .pinMux = GPT_PIN_3B, },
};

const GPTimerCC26XX_Config GPTimerCC26XX_config[CC2640R2_LAUNCHXL_GPTIMERPARTSCOUNT] = {
    { &gptimerCC26XXObjects[CC2640R2_LAUNCHXL_GPTIMER0], &gptimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_GPTIMER0A], GPT_A },
    { &gptimerCC26XXObjects[CC2640R2_LAUNCHXL_GPTIMER0], &gptimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_GPTIMER0B], GPT_B },
    { &gptimerCC26XXObjects[CC2640R2_LAUNCHXL_GPTIMER1], &gptimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_GPTIMER1A], GPT_A },
    { &gptimerCC26XXObjects[CC2640R2_LAUNCHXL_GPTIMER1], &gptimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_GPTIMER1B], GPT_B },
    { &gptimerCC26XXObjects[CC2640R2_LAUNCHXL_GPTIMER2], &gptimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_GPTIMER2A], GPT_A },
    { &gptimerCC26XXObjects[CC2640R2_LAUNCHXL_GPTIMER2], &gptimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_GPTIMER2B], GPT_B },
    { &gptimerCC26XXObjects[CC2640R2_LAUNCHXL_GPTIMER3], &gptimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_GPTIMER3A], GPT_A },
    { &gptimerCC26XXObjects[CC2640R2_LAUNCHXL_GPTIMER3], &gptimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_GPTIMER3B], GPT_B },
};

/*
 *  =============================== I2C ===============================
*/
/*#include <ti/drivers/I2C.h>
#include <ti/drivers/i2c/I2CCC26XX.h>

I2CCC26XX_Object i2cCC26xxObjects[CC2640R2_LAUNCHXL_I2CCOUNT];

const I2CCC26XX_HWAttrsV1 i2cCC26xxHWAttrs[CC2640R2_LAUNCHXL_I2CCOUNT] = {
    {
        .baseAddr    = I2C0_BASE,
        .powerMngrId = PowerCC26XX_PERIPH_I2C0,
        .intNum      = INT_I2C_IRQ,
        .intPriority = ~0,
        .swiPriority = 0,
        .sdaPin      = CC2640R2_LAUNCHXL_I2C0_SDA0,
        .sclPin      = CC2640R2_LAUNCHXL_I2C0_SCL0,
    }
};

const I2C_Config I2C_config[CC2640R2_LAUNCHXL_I2CCOUNT] = {
    {
        .fxnTablePtr = &I2CCC26XX_fxnTable,
        .object      = &i2cCC26xxObjects[CC2640R2_LAUNCHXL_I2C0],
        .hwAttrs     = &i2cCC26xxHWAttrs[CC2640R2_LAUNCHXL_I2C0]
    },
};

const uint_least8_t I2C_count = CC2640R2_LAUNCHXL_I2CCOUNT;

/*
 *  =============================== I2S ===============================
*/
/*#include <ti/drivers/I2S.h>
#include <ti/drivers/i2s/I2SCC26XX.h>

I2SCC26XX_Object i2sCC26XXObjects[CC2640R2_LAUNCHXL_I2SCOUNT];

const I2SCC26XX_HWAttrs i2sCC26XXHWAttrs[CC2640R2_LAUNCHXL_I2SCOUNT] = {
    {
        .pinSD1      =  CC2640R2_LAUNCHXL_I2S_ADI,
        .pinSD0      =  CC2640R2_LAUNCHXL_I2S_ADO,
        .pinSCK      =  CC2640R2_LAUNCHXL_I2S_BCLK,
        .pinMCLK     =  CC2640R2_LAUNCHXL_I2S_MCLK,
        .pinWS       =  CC2640R2_LAUNCHXL_I2S_WCLK,
        .intPriority = ~0,
    }
};

const I2S_Config I2S_config[CC2640R2_LAUNCHXL_I2SCOUNT] = {
    {
        .object      = &i2sCC26XXObjects[CC2640R2_LAUNCHXL_I2S0],
        .hwAttrs     = &i2sCC26XXHWAttrs[CC2640R2_LAUNCHXL_I2S0]
    },
};

const uint_least8_t I2S_count = CC2640R2_LAUNCHXL_I2SCOUNT;

/*
 *  =============================== NVS ===============================
 */
#include <ti/drivers/NVS.h>
#include <ti/drivers/nvs/NVSSPI25X.h>
#include <ti/drivers/nvs/NVSCC26XX.h>

#define NVS_REGIONS_BASE 0x1A000
#define SECTORSIZE       0x1000
#define REGIONSIZE       (SECTORSIZE * 4)

#ifndef Board_EXCLUDE_NVS_INTERNAL_FLASH

/*
 * Reserve flash sectors for NVS driver use by placing an uninitialized byte
 * array at the desired flash address.
 */
#if defined(__TI_COMPILER_VERSION__)

/*
 * Place uninitialized array at NVS_REGIONS_BASE
 */
#pragma LOCATION(flashBuf, NVS_REGIONS_BASE);
#pragma NOINIT(flashBuf);
static char flashBuf[REGIONSIZE];

#elif defined(__IAR_SYSTEMS_ICC__)

/*
 * Place uninitialized array at NVS_REGIONS_BASE
 */
static __no_init char flashBuf[REGIONSIZE] @ NVS_REGIONS_BASE;

#elif defined(__GNUC__)

/*
 * Place the flash buffers in the .nvs section created in the gcc linker file.
 * The .nvs section enforces alignment on a sector boundary but may
 * be placed anywhere in flash memory.  If desired the .nvs section can be set
 * to a fixed address by changing the following in the gcc linker file:
 *
 * .nvs (FIXED_FLASH_ADDR) (NOLOAD) : AT (FIXED_FLASH_ADDR) {
 *      *(.nvs)
 * } > REGION_TEXT
 */
__attribute__ ((section (".nvs")))
static char flashBuf[REGIONSIZE];

#endif

/* Allocate objects for NVS Internal Regions */
NVSCC26XX_Object nvsCC26xxObjects[1];

/* Hardware attributes for NVS Internal Regions */
const NVSCC26XX_HWAttrs nvsCC26xxHWAttrs[1] = {
    {
        .regionBase = (void *)flashBuf,
        .regionSize = REGIONSIZE,
    },
};

#endif /* Board_EXCLUDE_NVS_INTERNAL_FLASH */

#ifndef Board_EXCLUDE_NVS_EXTERNAL_FLASH

#define SPISECTORSIZE    0x1000
#define SPIREGIONSIZE    (SPISECTORSIZE * 32)
#define VERIFYBUFSIZE    64

static uint8_t verifyBuf[VERIFYBUFSIZE];

/* Allocate objects for NVS External Regions */
NVSSPI25X_Object nvsSPI25XObjects[1];

/* Hardware attributes for NVS External Regions */
const NVSSPI25X_HWAttrs nvsSPI25XHWAttrs[1] = {
    {
        .regionBaseOffset = 0,
        .regionSize = SPIREGIONSIZE,
        .sectorSize = SPISECTORSIZE,
        .verifyBuf = verifyBuf,
        .verifyBufSize = VERIFYBUFSIZE,
        .spiHandle = NULL,
        .spiIndex = 0,
        .spiBitRate = 4000000,
        .spiCsnGpioIndex = CC2640R2_LAUNCHXL_GPIO_SPI_FLASH_CS,
        .statusPollDelayUs = 100,
    },
};

#endif /* Board_EXCLUDE_NVS_EXTERNAL_FLASH */

/* NVS Region index 0 and 1 refer to NVS and NVS SPI respectively */
const NVS_Config NVS_config[CC2640R2_LAUNCHXL_NVSCOUNT] = {
#ifndef Board_EXCLUDE_NVS_INTERNAL_FLASH
    {
        .fxnTablePtr = &NVSCC26XX_fxnTable,
        .object = &nvsCC26xxObjects[0],
        .hwAttrs = &nvsCC26xxHWAttrs[0],
    },
#endif
#ifndef Board_EXCLUDE_NVS_EXTERNAL_FLASH
    {
        .fxnTablePtr = &NVSSPI25X_fxnTable,
        .object = &nvsSPI25XObjects[0],
        .hwAttrs = &nvsSPI25XHWAttrs[0],
    },
#endif
};

const uint_least8_t NVS_count = CC2640R2_LAUNCHXL_NVSCOUNT;

/*
 *  =============================== PIN ===============================
 */
#include <ti/drivers/PIN.h>
#include <ti/drivers/pin/PINCC26XX.h>

const PIN_Config KekoGpioInitTable[] = {

    //BUTTON_ADC_PIN        | PIN_INPUT_EN | PIN_NOPULL,
    //CAN_RST_PIN           | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW   | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    //CAN_INT_PIN           | PIN_INPUT_EN | PIN_PULLUP,
    //LED_PIN               | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW   | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    //CAN_NWRQ_RFDATA_PIN   | PIN_INPUT_EN | PIN_PULLUP,
    //CAN_SPI_NCS_PIN       | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW   | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    //CAN_SPI_NCLK_PIN      | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW   | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    //DATA_OUT_PIN          | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW   | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    //DATA_IN_PIN           | PIN_INPUT_EN | PIN_PULLUP,
    //HBRIDGE_CSENSE_PIN    | PIN_INPUT_EN | PIN_NOPULL,
    //HBRIDGE_PSENSE_PIN    | PIN_INPUT_EN | PIN_NOPULL,
    //HBRIDGE_B_PIN         | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW   | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    //HBRIDGE_A_PIN         | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW   | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    //HBRIDGE_EN_PIN        | PIN_INPUT_EN  | PIN_PULLUP | PIN_HYSTERESIS,
    //HBRIDGE_PWM_PIN       | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW   | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    PIN_TERMINATE
};

const PINCC26XX_HWAttrs PINCC26XX_hwAttrs = {
    .intPriority = ~0,
    .swiPriority = 0
};

/*
 *  =============================== Power ===============================
 */
#include <ti/drivers/Power.h>
#include <ti/drivers/power/PowerCC26XX.h>

const PowerCC26XX_Config PowerCC26XX_config = {
    .policyInitFxn      = NULL,
    .policyFxn          = &PowerCC26XX_standbyPolicy,
    .calibrateFxn       = &PowerCC26XX_calibrate,
    .enablePolicy       = true,
    .calibrateRCOSC_LF  = true,
    .calibrateRCOSC_HF  = true,
};

/*
 *  =============================== PWM ===============================
 *  Remove unused entries to reduce flash usage both in Board.c and Board.h
 */
#include <ti/drivers/PWM.h>
#include <ti/drivers/pwm/PWMTimerCC26XX.h>

PWMTimerCC26XX_Object pwmtimerCC26xxObjects[CC2640R2_LAUNCHXL_PWMCOUNT];

const PWMTimerCC26XX_HwAttrs pwmtimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_PWMCOUNT] = {
    { .pwmPin = CC2640R2_LAUNCHXL_PWMPIN0, .gpTimerUnit = CC2640R2_LAUNCHXL_GPTIMER0A },
    { .pwmPin = CC2640R2_LAUNCHXL_PWMPIN1, .gpTimerUnit = CC2640R2_LAUNCHXL_GPTIMER0B },
    { .pwmPin = CC2640R2_LAUNCHXL_PWMPIN2, .gpTimerUnit = CC2640R2_LAUNCHXL_GPTIMER1A },
    { .pwmPin = CC2640R2_LAUNCHXL_PWMPIN3, .gpTimerUnit = CC2640R2_LAUNCHXL_GPTIMER1B },
    { .pwmPin = CC2640R2_LAUNCHXL_PWMPIN4, .gpTimerUnit = CC2640R2_LAUNCHXL_GPTIMER2A },
    { .pwmPin = CC2640R2_LAUNCHXL_PWMPIN5, .gpTimerUnit = CC2640R2_LAUNCHXL_GPTIMER2B },
    { .pwmPin = CC2640R2_LAUNCHXL_PWMPIN6, .gpTimerUnit = CC2640R2_LAUNCHXL_GPTIMER3A },
    { .pwmPin = CC2640R2_LAUNCHXL_PWMPIN7, .gpTimerUnit = CC2640R2_LAUNCHXL_GPTIMER3B },
};

const PWM_Config PWM_config[CC2640R2_LAUNCHXL_PWMCOUNT] = {
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2_LAUNCHXL_PWM0], &pwmtimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_PWM0] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2_LAUNCHXL_PWM1], &pwmtimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_PWM1] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2_LAUNCHXL_PWM2], &pwmtimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_PWM2] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2_LAUNCHXL_PWM3], &pwmtimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_PWM3] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2_LAUNCHXL_PWM4], &pwmtimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_PWM4] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2_LAUNCHXL_PWM5], &pwmtimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_PWM5] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2_LAUNCHXL_PWM6], &pwmtimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_PWM6] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2_LAUNCHXL_PWM7], &pwmtimerCC26xxHWAttrs[CC2640R2_LAUNCHXL_PWM7] },
};

const uint_least8_t PWM_count = CC2640R2_LAUNCHXL_PWMCOUNT;

/*
 *  =============================== RF Driver ===============================
 */
#include <ti/drivers/rf/RF.h>

const RFCC26XX_HWAttrsV2 RFCC26XX_hwAttrs = {
    .hwiPriority        = ~0,       /* Lowest HWI priority */
    .swiPriority        = 0,        /* Lowest SWI priority */
    .xoscHfAlwaysNeeded = true,     /* Keep XOSC dependency while in standby */
    .globalCallback     = NULL,     /* No board specific callback */
    .globalEventMask    = 0         /* No events subscribed to */
};

/*
 *  =============================== SD ===============================
 */
/*#include <ti/drivers/SD.h>
#include <ti/drivers/sd/SDSPI.h>

SDSPI_Object sdspiObjects[CC2640R2_LAUNCHXL_SDCOUNT];

const SDSPI_HWAttrs sdspiHWAttrs[CC2640R2_LAUNCHXL_SDCOUNT] = {
    {
        .spiIndex = CC2640R2_LAUNCHXL_SPI0,
        .spiCsGpioIndex = CC2640R2_LAUNCHXL_SDSPI_CS
    }
};

const SD_Config SD_config[CC2640R2_LAUNCHXL_SDCOUNT] = {
    {
        .fxnTablePtr = &SDSPI_fxnTable,
        .object = &sdspiObjects[CC2640R2_LAUNCHXL_SDSPI0],
        .hwAttrs = &sdspiHWAttrs[CC2640R2_LAUNCHXL_SDSPI0]
    },
};

const uint_least8_t SD_count = CC2640R2_LAUNCHXL_SDCOUNT;

/*
 *  =============================== SPI DMA ===============================
 */
/*#include <ti/drivers/SPI.h>
#include <ti/drivers/spi/SPICC26XXDMA.h>

SPICC26XXDMA_Object spiCC26XXDMAObjects[CC2640R2_LAUNCHXL_SPICOUNT];

/*
 * NOTE: The SPI instances below can be used by the SD driver to communicate
 * with a SD card via SPI.  The 'defaultTxBufValue' fields below are set to 0xFF
 * to satisfy the SDSPI driver requirement.
 */
/*const SPICC26XXDMA_HWAttrsV1 spiCC26XXDMAHWAttrs[CC2640R2_LAUNCHXL_SPICOUNT] = {
    {
        .baseAddr           = SSI0_BASE,
        .intNum             = INT_SSI0_COMB,
        .intPriority        = ~0,
        .swiPriority        = 0,
        .powerMngrId        = PowerCC26XX_PERIPH_SSI0,
        .defaultTxBufValue  = 0xFF,
        .rxChannelBitMask   = 1<<UDMA_CHAN_SSI0_RX,
        .txChannelBitMask   = 1<<UDMA_CHAN_SSI0_TX,
        .mosiPin            = CC2640R2_LAUNCHXL_SPI0_MOSI,
        .misoPin            = CC2640R2_LAUNCHXL_SPI0_MISO,
        .clkPin             = CC2640R2_LAUNCHXL_SPI0_CLK,
        .csnPin             = CC2640R2_LAUNCHXL_SPI0_CSN,
        .minDmaTransferSize = 10
    },
    {
        .baseAddr           = SSI1_BASE,
        .intNum             = INT_SSI1_COMB,
        .intPriority        = ~0,
        .swiPriority        = 0,
        .powerMngrId        = PowerCC26XX_PERIPH_SSI1,
        .defaultTxBufValue  = 0xFF,
        .rxChannelBitMask   = 1<<UDMA_CHAN_SSI1_RX,
        .txChannelBitMask   = 1<<UDMA_CHAN_SSI1_TX,
        .mosiPin            = CC2640R2_LAUNCHXL_SPI1_MOSI,
        .misoPin            = CC2640R2_LAUNCHXL_SPI1_MISO,
        .clkPin             = CC2640R2_LAUNCHXL_SPI1_CLK,
        .csnPin             = CC2640R2_LAUNCHXL_SPI1_CSN,
        .minDmaTransferSize = 10
    }
};

const SPI_Config SPI_config[CC2640R2_LAUNCHXL_SPICOUNT] = {
    {
         .fxnTablePtr = &SPICC26XXDMA_fxnTable,
         .object      = &spiCC26XXDMAObjects[CC2640R2_LAUNCHXL_SPI0],
         .hwAttrs     = &spiCC26XXDMAHWAttrs[CC2640R2_LAUNCHXL_SPI0]
    },
    {
         .fxnTablePtr = &SPICC26XXDMA_fxnTable,
         .object      = &spiCC26XXDMAObjects[CC2640R2_LAUNCHXL_SPI1],
         .hwAttrs     = &spiCC26XXDMAHWAttrs[CC2640R2_LAUNCHXL_SPI1]
    },
};

const uint_least8_t SPI_count = CC2640R2_LAUNCHXL_SPICOUNT;

/*
 *  =============================== UART ===============================
 */
#include <ti/drivers/UART.h>
#include <ti/drivers/uart/UARTCC26XX.h>

UARTCC26XX_Object uartCC26XXObjects[CC2640R2_LAUNCHXL_UARTCOUNT];

uint8_t uartCC26XXRingBuffer[CC2640R2_LAUNCHXL_UARTCOUNT][32];

const UARTCC26XX_HWAttrsV2 uartCC26XXHWAttrs[CC2640R2_LAUNCHXL_UARTCOUNT] = {
    {
        .baseAddr       = UART0_BASE,
        .powerMngrId    = PowerCC26XX_PERIPH_UART0,
        .intNum         = INT_UART0_COMB,
        .intPriority    = ~0,
        .swiPriority    = 0,
        .txPin          = CC2640R2_LAUNCHXL_UART_TX,
        .rxPin          = CC2640R2_LAUNCHXL_UART_RX,
        .ctsPin         = PIN_UNASSIGNED,
        .rtsPin         = PIN_UNASSIGNED,
        .ringBufPtr     = uartCC26XXRingBuffer[CC2640R2_LAUNCHXL_UART0],
        .ringBufSize    = sizeof(uartCC26XXRingBuffer[CC2640R2_LAUNCHXL_UART0]),
        .txIntFifoThr   = UARTCC26XX_FIFO_THRESHOLD_1_8,
        .rxIntFifoThr   = UARTCC26XX_FIFO_THRESHOLD_4_8,
        .errorFxn       = NULL
    }
};

const UART_Config UART_config[CC2640R2_LAUNCHXL_UARTCOUNT] = {
    {
        .fxnTablePtr = &UARTCC26XX_fxnTable,
        .object      = &uartCC26XXObjects[CC2640R2_LAUNCHXL_UART0],
        .hwAttrs     = &uartCC26XXHWAttrs[CC2640R2_LAUNCHXL_UART0]
    },
};

const uint_least8_t UART_count = CC2640R2_LAUNCHXL_UARTCOUNT;

/*
 *  =============================== UDMA ===============================
 */
/*#include <ti/drivers/dma/UDMACC26XX.h>

UDMACC26XX_Object udmaObjects[CC2640R2_LAUNCHXL_UDMACOUNT];

const UDMACC26XX_HWAttrs udmaHWAttrs[CC2640R2_LAUNCHXL_UDMACOUNT] = {
    {
        .baseAddr    = UDMA0_BASE,
        .powerMngrId = PowerCC26XX_PERIPH_UDMA,
        .intNum      = INT_DMA_ERR,
        .intPriority = ~0
    }
};

const UDMACC26XX_Config UDMACC26XX_config[CC2640R2_LAUNCHXL_UDMACOUNT] = {
    {
         .object  = &udmaObjects[CC2640R2_LAUNCHXL_UDMA0],
         .hwAttrs = &udmaHWAttrs[CC2640R2_LAUNCHXL_UDMA0]
    },
};



/*
 *  =============================== Watchdog ===============================
 */
#include <ti/drivers/Watchdog.h>
#include <ti/drivers/watchdog/WatchdogCC26XX.h>

WatchdogCC26XX_Object watchdogCC26XXObjects[CC2640R2_LAUNCHXL_WATCHDOGCOUNT];

const WatchdogCC26XX_HWAttrs watchdogCC26XXHWAttrs[CC2640R2_LAUNCHXL_WATCHDOGCOUNT] = {
    {
        .baseAddr    = WDT_BASE,
        .reloadValue = 1000 /* Reload value in milliseconds */
    },
};

const Watchdog_Config Watchdog_config[CC2640R2_LAUNCHXL_WATCHDOGCOUNT] = {
    {
        .fxnTablePtr = &WatchdogCC26XX_fxnTable,
        .object      = &watchdogCC26XXObjects[CC2640R2_LAUNCHXL_WATCHDOG0],
        .hwAttrs     = &watchdogCC26XXHWAttrs[CC2640R2_LAUNCHXL_WATCHDOG0]
    },
};

const uint_least8_t Watchdog_count = CC2640R2_LAUNCHXL_WATCHDOGCOUNT;

/*
 *  Board-specific initialization function to disable external flash.
 *  This function is defined in the file CC2640R2_LAUNCHXL_fxns.c
 */
extern void Board_initHook(void);

/*
 *  ======== CC2640R2_LAUNCHXL_initGeneral ========
 */
void CC2640R2_LAUNCHXL_initGeneral(void)
{
    Power_init();

    if (PIN_init(KekoGpioInitTable) != PIN_SUCCESS) {
        /* Error with PIN_init */
        while (1);
    }

    /* Perform board-specific initialization */
    //Board_initHook();
}

/*
 *  ======== Board_init ========
 */
void Board_init(void)
{
    CC2640R2_LAUNCHXL_initGeneral();
}
5504.Board.h

  • Hi Dheigo,

    SysConfig should be available as preview in the 3.40 SDK.

    As for your configuration, have a look at the "adcCC26xxHWAttrs" structure in the CC2640R2_LAUNCHXL.c file. To be more precise, the field 

    ".adcCompBInput" which defines the input to the ADC. In your case, it is set to ADC_COMPB_IN_VDDS for both your ADC configurations which basically means you are measuring VDDS and no the actual pin.
    Note that there is only a few IOs that support AUX (and thus ADC) on the CC2640R2, you can read about this in the Technical Reference Manual, Table 11-2.
    I recommend you have a look at the "adcsinglechannel" example to see how the ADC HwAttrs is setup.
  • Hi M-W,

    I am using pins DIO_0 and DIO_3 to read the analog signals.

    According to the table informed by you, these pins do not support ADC.

    So that's the problem.

    Thank you for the answer.