Part Number: CC2564MODA
Dear Sr/Mrs.
We are trying to certify CC2564moda in our custom application.
We have to do FCC tests with two-way radiated (with chip antenna) and conducted (with SMA cable) in countries Corea, Taiwan, China,Mexic.
We have started with this page https://processors.wiki.ti.com/index.php/CC256x_FCC_Testing_Guide#Introduction and with HCI tester we are capable to send message to both CC2564moda successfully ( in our custom application we have two of them in the same PCB, master and slave)
The problem is sometimes the frequency that should be given by module is not the exact one we want. For example
Example 2. GFSK, PN9, 78 (2479 MHz), 15:
We send test commands with HCI TESTER by UART, and in some pcbs for example with master we have similar signal, but with slave the signal is shifted (to 20 channels left and doesn't have the same amplitude)
We send this commands:
Send_HCI_Enable_Device_Under_Test_Mode
Wait_HCI_Command_Complete_Enable_Device_Under_Test_Mode_Event 5000, any, HCI_Enable_Device_Under_Test_Mode, 0x00
# Example 2. GFSK, PN9, 78 (2479 MHz), 15
Send_HCI_VS_DRPb_Tester_Con_TX 0xFD84, 0x01, 0x00, 0x4E, 15, 0x00000000, 0x00000000
Wait_HCI_Command_Complete_VS_DRPb_Tester_Con_TX_Event 5000, any, HCI_VS_DRPb_Tester_Con_TX, 0x00
Any help and extra information to solve our problem (frequency shifting ) will be appreciated.
Regards,German