Other Parts Discussed in Thread: CC2652R, CC2642R
Hi,
from the SIMPLELINK-CC2640R2-SDK docs I learned that RTLS demos needs TI BLE stack on all three type of BLE devices (master, slave and passive). Probably because of including ToF to support AoA precision. But is is possible to use one or more SIMPLELINK-CC2640R2-SDK devices with antenna array to track a 3rd party device, let's say a mobile phone or simple BLE 5.1 battery tag, that will only transmit advertise packets with CTE enabled? The scanner would only know the BLE MAC to recognize which device to track. I think that in principle it should work. Can be TI RTLS toolbox configured to do this or does it need to be rewritten?