Part Number: BOOSTXL-AOA
Hello Ti,
I have conducted an angle of arrival experiment in various environments such as indoor-outdoor and all. I have taken all the instructions provided and thank you for that. Now I have a few concerns regarding that.
1) Where should the master be placed(ideally ) when the slave or sender is placed 1m above and 2.8 m far from the sender.
2) I have conducted experiments and got these values i.e., 40 degrees as the angle even though I have measured manually it to be 0. I have attached an image below please have a look at it
3) whenever I change the sender the angle changes but it does change as per the angle it should be
It usually gives values from 50 - (-50) instead of -180- (-180). Please let me know how to correct this.