This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Why the distance of BLE5 Long Range Mode is shorter than TI official test?

Part Number: CC2640R2F


Hi Team ,

        We have used 2 TI lauchpad in BLE connecting status to test the distance of BLE5 Long Range Mode and we found the distance in outdoor open environments is just 150-170m. Compared with the test data by TI (400m in indoor open environments),Our distance is too short. Can you help to guide how to increase the distance ? Thank you !

  

        The following are our sets:  

        SDK Version:simplelink_cc2640r2_sdk_3_20_00_21 

        Example : Simplecentral & Simpleperipheral  

        Txpower : 5dbm 

        MTU: 65

        Connection interval: 100ms

        Latency: 0 

        Connection Timeout: 3s

        Modified the Phy & Txpower : Via function :  HCI_LE_SetPhyCmd(connHandle, 0, HCI_PHY_CODED, HCI_PHY_CODED, LL_PHY_OPT_S8)  

                                                                                  HCI_EXT_SetTxPowerCmd(HCI_EXT_TX_POWER_5_DBM)