This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: on CC26x2 LP

Part Number: CC2642R
Other Parts Discussed in Thread: CC2652R

hi,

we have a new project based on BLE CC2642R and are using CC26x2 LP for the SW development.

Later on we wish to move to the final version with CC2642R.

Is there any guideline how to migrate to CC2642R starting from the CC2652?

Can we just replace the IC on the launchpad to test the porting?

thanks a lot in advance

KR

Vincenzo

  • CC2642R is a subset of CC2652R where the latter support multiple protocols but the former supports only BLE and proprietary applications. Meaning that if the code does not use some of  the protocols only supported on CC2652R you will have no issues using the exact same code on a new device. 

    If you want to test the porting, swapping the chip on the Launchpad is an option.